Part Number: UCC27712 Hi. there.
I'm DH.Kim
I'm reviewing the totem pole PFC using TIDA-00961.
and attached file is the circuit of TIDA-00961.
please see the attached file and page 2(two) with UCC27712DR(U102)
there are L1 and H1 in I.C
The input…
Part Number: TIDA-00961 Hello!
Cant open the reference project? According the Guide I imported project and click on main.syscfg file but than I have a message: Device Not Found: F28004x. If I then clcick ok I will on the page where I can't choose board…
Hi
This Inoue
I have a question. in epwm.h
static inline void EPWM_setActionQualifierContSWForceAction(uint32_t base, EPWM_ActionQualifierOutputModule epwmOutput, EPWM_ActionQualifierSWOutput output) { // // Check the arguments // ASSERT(EPWM_isBaseValid…
Part Number: TIDA-00961 Tool/software: Code Composer Studio Since there is no prototype for sale, what do I need if I want to do some experiments?
Moreever, I found that the TMDSCNCD280049C- F280049C controlCARD Evaluation Module doesn't have 14pin JTAG…
Part Number: TIDA-00961 Hello, recently I am rebuilding the TIDA-00961 project and have some questions about the schematic.
Q1.There are two blank signals connected to the MCU. And one of them is short to ACTIVE_PWM1. So which one is incorrect? Or both…
Part Number: TIDA-00961 Hi sir,
I an interesting in reference design TIDA 00961.
I want to make the board with the exposed Gerber data of the reference design TIDA 00961,
and I was told that it cannot manufacture because of the overseas standard from two…
Part Number: TIDA-00961 Tool/software: Code Composer Studio I used TIDA-00961 solution on my project.
I used 64Pin tms320f280049c chip.
and I used 3 phase interleaved Totem pole PFC, Critical conduction mode or DCM.
the code based on TIDA-00961 solution…
Part Number: TMS320F280049C Other Parts Discussed in Thread: C2000WARE Hi
The fast interrupt routine interrupt void controlISR (void) does not start in the pfc2philtrmttpl project. Tell me where the interrupts of this routine are triggered and where they…
Part Number: TIDA-00961 Tool/software: Code Composer Studio Hello, I have one question about TIDA-00961.
I made the CRM Totem-Pole PFC hardware by referring to the TIDA-00961 schematic.
Using this hardware, I'm currently testing open-loop operation in…
Part Number: TIDA-00961 Tool/software: Code Composer Studio Hello, recently I have been studying the TIDA-00961 [High-Efficiency, 1.6-kW, High-Density, GaN-Based, 1-MHz CrM Totem-Pole PFC Converter Reference] and met many questions.
Firstly, I will tell…