Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 , Hello,
In TIDA-010208 (Page-6), the writer has used an external circuit (Q28 and peripheral) to turn off the DSG FET, we wanted to understand the advantage of it. Since, one could…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 , Hi TI's experts,
1. When I design the schematic diagram, because the reference ground inside the AFE is B-, and the reference ground of the externally connected MCU circuit is P-. Confused…
Part Number: BQ76942 Other Parts Discussed in Thread: TIDA-010208 , BQSTUDIO , BQ34Z100-R2 I had a few questions revolving around the BQ76942 and supplemental circuitry. I'm working to build a 10s pack that requires the following:
15A Continuous Discharge…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 Hi There,
I am referring "TIDA-010208" and I just need to use reverse protection and not the Q28 and its related circuitry.
I want to know, exactly which components I need to remove…
Hello Cong,
I understand now. We often refer to your "GND" as "PACK-".
Vss should always be referenced to BAT-, this is how the part was designed to work.
It should not be placed in PACK-. I originally missed that this is how you have it placed…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 , EV2400 , BQSTUDIO We are using the evaluation board TIDA-010208.
We have mounted all AFE components as per schematic. 1.8V is at Pin number 24 ( REG18 ) continuously when 60 voltage…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208
Hi
The customer test with the BQ76952 board which they designed. They use the non-contact ± 15kV to test the CAN communication port, and find 8. 9. 10 pin damage.
Total test with…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 , Hello
Matt directed my to the TIDA-010208 design and the pin diagram in my related thread.
Given the abs max shows minimum voltage on the VC0 pin of -0.3V, a BAT43WS-7 will protect…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 Hi There,
We are planning to use BQ76952 chips for a 22cell BMS and I would like to know if the pack voltage is around 90VDC then what should be the ratings of Q29 and D42 ?
I would…
Part Number: BQ76942 Other Parts Discussed in Thread: TIDA-010208 The app note SLUAA81 says:
A Zener diode is needed to protect the external FET gate from pack transients. For example, in the event of a short across the pack in a 10-cell battery, Cell…