Part Number: TIDA-01022 Other Parts Discussed in Thread: ADC12DJ3200 , Hi Team,
I used TIDA-01022 and two TSW14J57 to verify ADC12DJ3200 synchronization. HSDC PRO uses trigger mode, and the phase between the two ADCs sometimes jumps by one LMFC cycle. Is…
Part Number: TIDA-01022 Hi Team
I am using the TIDA-01022 as reference for my design. i have several questions
1. What is the cut of frequency of the input analog filter?
2. Why do you need the analog filtering of inductor and capacitors?The input stage…
Part Number: TIDA-01022 Hi Expert,
Our customer is developing 821 for a gateway project. They are requesting BRD file for layout reference. Could you please kindly provide? Thanks.
BR,
Elec Cheng
Part Number: TIDA-01022 Other Parts Discussed in Thread: TIDA-01027 Hi, support team
My customer has the questions as follow:
Could you provide 3D CAD STEP format files of the following products/electronic boards: (or equivalent 3D neutral format such…
Part Number: TIDA-01022 Other Parts Discussed in Thread: ADS5296A Hello All,
I have employed two ADCs in my design like those in TIDA-01022 and I have questions regarding AGND and DGND in the layout. I greatly appreciate if you would help me with questions…
Hi Michael,
LMK04828 clock generation and distribution device with JESD204B compliant clocking , the device has 2 PLL and clock dividers to generate JESD compliant clock up to 7 output pair (DCLK and SYSREF). It can accept the reference clock input from…
Hi Michael,
TIDA-01022 has four channels(2x ADC12DJ3200) and each channel can operate 3.2 Gsps at dual channel mode , 6.4 Gsps at single channel mode.
Also 2xADC12DJ3200 can be interleaved onboard to increase sample rate 12.8 Gsps.
Let me know what…
1. What bandwidth, sample rate you are looking for your application
sub-6GHz, 800MHz bandwidth
2. Application requires AC or DC coupling ?
AC coupling
3. Did you want to use ADC digital feature (like DDC (decimation mode), NCO )
yes
4…
Hi Michael,
Please find the default jumper positions and its functions of TIDA-01022 below and we will update those information in the design guide. let me know If you required any further information.
TIDA-01022 Jumpers.pdf