Part Number: TIDA-01028 Hi,
I think the symobol of T3 is wrong on schematic diagram. (compare with T2 and T1 /they have the same pinouts/).We just built this board and the Flying probe machine was failing on the T3 test which were set based on schematic…
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: TIDA-01028 , TIDA-01022 , ADC12DJ5200RF
Hi,
I am planning to design a 20GSPS high speed osciloscope using 4 interleaving ADC12DJ3200. In TIDA-01028 user guide,Figures 31 and 32 show the ADC performance…
Part Number: TIDA-01028 I would like to know the part numbers of capacitors used in TIDA-01028 board having the following ratings
(1) 100nF, 50V
(2) 1uF, 16V
(3) 10uF, 25V
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: TIDA-01022 , LMK04828 , LMX2572 , TIDA-010122 , TSW14J57EVM , TIDA-01028 Hi,
We have a custom board with 2 ADC12DJ3200 ADCs and Kintex UltraScale FPGA from Xilinx. We are using JMODE 11.
The data captured…
Part Number: ADC12DJ5200RF Other Parts Discussed in Thread: TIDA-010128 , TIDA-01028
Hi,
Wrt my previous question on crc errors in JESD204C data, as per the suggestion provided, after running at lower sampling rates the frequency of occurrence of crc errors…
Part Number: ADC12DJ5200RF Other Parts Discussed in Thread: TIDA-01028 , I am using two ADC12DJ5200RF in dual channel mode. (Schematic reference: TIDA-01028). LMK, LMXs and ADCs(JMODE3) are configured through SPI via FMC+.
This ADC board is connected to…
Michael,
Another thing I'd like to add is I've been referencing TIDA-01028 for help with my own design. It uses the ADC12DJ3200 with the LMH5401 on the frontend with +/- 2.5V rails.
Part Number: LMK04828 Other Parts Discussed in Thread: ADC12DJ3200 , TIDA-01028 Hi TI,
We will be using LMK04828 for generating Sysref clocks for ADC12DJ3200 and for generating GBTCLK,Sysref clock and Referenc clock for virtex-7 FPGA.
Now ADC12DJ3200 sysref…
Hi Lalit,
Please look at this reference design that utilizes two ADC12DJ3200s. While you are looking to integrate 3 ADCs, this should provide a good feel for component placement.
http://www.ti.com/tool/TIDA-01028
Best Regards,
Dan
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: LMK04828 , LMX2582 , TIDA-01028 Hi TI,
We are using three ADC12DJ3200 in our design.
In eval board for ADC12DJ3200, single ground is used for all components viz. ADC12DJ3200, LMK04828,LMX2582 and…