Part Number: TIDA-01168
Error connecting to the target: (Error -233 @ 0x0) The JTAG IR and DR scan-paths cannot circulate bits, they may be broken. An attempt to scan the JTAG scan-path has failed. The target's JTAG scan-path appears to be broken with…
Part Number: TIDA-01168 Other Parts Discussed in Thread: TMS320F28027 ,
I have made the board exactly as it is in TIDA-01168, and I am currently debugging with example code in TIDA-01168 on the TMS320F28027 using CCS V7 and XDSV3 EMULATOR. During this…
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170-Q1 Hi team,
Customer is build an automotive battery pack, and they want our the reference EVM of TIDA-01168 for testing. So, do we have any method to get this EVM of TIDA-01168?
Thanks!
Part Number: TIDA-01168 Greetings -
Please let me know if information is available regarding the optimized layout mentioned in "TIDA-10068: Board Size Information", January 22, 2019.
"I have an experimental design with LM5170-Q1 in works…
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170 , LM5170-Q1 , SFRA We have stability issues with our converter which is based on the TIDA-01168. What is the correlation between the coefficients used in the software (Buck mode shown below…
Part Number: TIDA-01168 Other Parts Discussed in Thread: TMS320F28027 , We are running slightly modified software of the TIDA-01168 for our application. There is now only a 4.7k pull-up resistor on the XRS pin of the TMS320F28027. The software has the BOR…
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170-Q1 Hello.
I created a TIDA-01168 based converter.
Please let me know because I have questions.
In 48VIN => 14VOUT operation, if you increase the load current,
A phenomenon occurs in which…
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170 , LM5060-Q1 , LM5060 , LM5170-Q1 , TIDA-01167 Hello.
Please tell me about TIDA-01168.
Q1: JAU275B Page55 has the following description.
>The jitter size is ± 3 × tADC_chan_sampl…
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170-Q1 Dear Sir,
Customer would refer TIDA-01168 to do low input voltage(like under 3V) for Cell application(1.5V/ 3V to 12V)
Could you kindly review & provide suggestion.
Thanks!
Steven
Part Number: TIDA-01168 Other Parts Discussed in Thread: LM5170-Q1 , Hi Team,
Can 2 independent TIDA-01168-type bidirectional converters (LM5170-Q1+C2000 implementing ACMC loop) be paralleled? The goal is to design a 1.5kW system that could be paralleled…