Part Number: LM5030 Other Parts Discussed in Thread: TIDA-01352 Hi Expert
For TIDA-01352
But I need to make some ultrasound application.
The spec of product is input voltage 12V, output voltage is +-100V , 50W.
The original design is for 24v input.
Do…
Part Number: TIDA-01352 Other Parts Discussed in Thread: LM5030 Hi,
I have built the reference bard design TIDA-01352 and I'm looking at the performances using an electronic load.
I cannot reach the performance given in the design guide TIDUCD8.PDF…
Part Number: TIDA-01352 Other Parts Discussed in Thread: LM5030 , DAC60004 Hi all,
We are promoting TIDA-01352, customer has following questions:
1. Why TIDA use non-isolation feedback while there is an isolation feedback on LM5030 datasheet? Do customer…
Part Number: TIDA-01352 Other Parts Discussed in Thread: TX7332 , , LM5030 , TIDA-00181 , LMZ34202 , LMZ34002 , LM3411 Hi, Our system will have 64 channels and need TX7332. Each TX7332 need 5 supply rails such as: 1. 1.8V Fixed supply rail
2. 5.0V Fixed supply…
Part Number: LM5030 Other Parts Discussed in Thread: TIDA-01352 Dear mr.
My questions:
1. I try to build power supply 400W, Vin=18V-29V to 300V with LM5030 and order for it planar transformer with next parameters: 500W, n=1:19, Lprimary1-3= 8.5uH (10kHz…
Part Number: TIDA-01352 Other Parts Discussed in Thread: DAC60004 , LM5030 Hi,
Initially, our ultrasound system is planning to support only B-MODE, CWD and PWD mode. Thus we don’t have Elastography mode that requires High voltage +/-150V with huge current…
Part Number: LM5030 Other Parts Discussed in Thread: TIDA-01352 Hi,
We got a question from the customer about LM5030. Could you help us?
[Question] They are considering using LM5030 based on TIDA-01352 at 14V input voltage. Thus they have to change some…
Part Number: TIDA-01352 Other Parts Discussed in Thread: LM5030 , TINA-TI
Hi,
Do anyone have TINA simulation files of any one of the following sections of TIDA-01352?
1.Positive HV Push Pull Power Supply section 2.Positive LV Push Pull Power Supply se…
Hi,
As your input voltage minimum is 8.5V compared to TIDA-01352 24V, the transformer turns ratio for TIDA-01352 Np:21Ns = 1:7.5, then yours should be Np:Ns = 1:(7.5 x 24/8.5) = 1: 21.2. Other parameters can be similar to TIDA-01352 transformer 750343547…
Hello Hunting,
Have you look at TIDA-01352? It can support up to 100W on each rail and uses LM5030 in push-pull configuration.
Regards,
Sanjay R. Pithadia