Part Number: TIDA-01417 Other Parts Discussed in Thread: UCC28740 , Hello,
we plan to do a new design with UCC28740. Do you've got some measures about Conductive EMI 230VAC according EN55015Q and EN55022A.
We found no measures in all documents. Did…
Other Parts Discussed in Thread: TIDA-01417 Hi
In ti designer TIDA-01417 , It is 30w BLDC application ,but one component has not detail file . that is T1 transformer . In bom , there is just 280UH
.
Can someone support this transformer detail paramtere? so I…
Hi Kamal,
Our reference designs, typically don't include PFC if the power level is below 75W. Here is another reference design to check out TIDA-01417 . Do you think this can work for you? You can always add in a PFC front-end the UCC28056 might be…
1) To see if TI has a AC/DC(PFC,under 100W, 90V~300V to 24V/3A) solution, I would ask on the appropriate e2e forum. As per TI designs that incorporate both the ac/dc stage and DRV10x drivers, i would look at the below designs. They are for DRV10983, which…