Part Number: TIDA-01495 Hi Team,
We are working with TIDA-01495 and we need you support on the following devices, can you please advise with details of them?
Can you please share datasheets?
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: TIDA-01495 We are planning to modify this design to work with output 28 V and Current 24A..
Please suggest suitable changes to incorporate with the above required output level
Part Number: TIDA-01495
Dear Sir,
We are planning to follow the TI design TIDA-01495 for 480 watt AC-DC converter..
In the technical specifications, it is mentioned that operating ambient temperature is from 25 to 55..
We are looking for industrial…
Part Number: TIDA-01495 Other Parts Discussed in Thread: UCC28063
Hi,
I have two queries in TIDA-01495
1. For an minimum input AC voltage range of 70VAC, please suggest the voltage divider to be connected to VINAC pin in UCC28063.
2. Is the design…
Other Parts Discussed in Thread: TIDA-01495 Hi Everyone ,
Do TI have PSPICE model for AC to DC power supply module .
Do anyone have TIDA-01495 module's pspice model file ? Want to check the performance of this TIDA-01495 model with LED driver .
Other Parts Discussed in Thread: TIDA-01495 , TIDA-010015 Hi Everyone,
Planning to use TIDA-01495 model reference design for our new development. But while cross verifying the datasheet , Design guide and Schematic, the reference values are not matched …
Part Number: TIDA-01495 Other Parts Discussed in Thread: UCC28063A Hello Ram sir ,
customer is planning to increase the maximum power rating of TIDA-01495 by an additional 100W .
Do you think the design and topology selected can still support .