Part Number: TIDA-01501 Dear sir,
Could you help provide below Transformer datasheet for TIDA-01501 BOM.
L1/ 7.5mH/ Common choke/ LianFeng Dongjin
L2/ 3mH/ Common choke/LianFeng Dongjin
L3/ 400uH/ PFC Choke/ LianFeng Dongjin]
L4/ 32.8uH/ LLC Resonant…
Part Number: TIDA-01501 Hi
I want to know the turn spec of trans & coil in TIDA-01501
L1: Common choke 7.5mH(T16)
L2: Common choke 3mH(T16)
L3: PFC coil 400uH(PQ3240)
L4: LLC Inductor 32.8uH(PQ2016)
T1: Trans 230uH(PQ3228)
Thanks
Part Number: TIDA-01501
Hello,
May you upload the specifications or the approval sheet of T1 please? In any case if you provide some info about the dimensions of it it would be enough.
Thanks in advance,
Amr
Part Number: TIDA-01501 Hello,
The PFC Choke L3 of 400uH has unfortunately no specified current Rating or Saturation Points? Would you please provide them?
I have looked in the uploaded pdf file for magnetics but also didn't find them.
Thanks,
A…
Part Number: TIDA-01501 Hello,
Some signals are not clear how they are connected.
-On the LLC stage schematic, it is unclear how V+ and V- of the LM258AD are connected. The components are named U2 and U10.
-What is U15?
-Is the Signal VTEMP in the LLC…
Part Number: TIDA-01501 Hello,
may I ask you please if you plan to offer the fully assembled board for sale in the future? When approximately?
Thank you,
Amr
Part Number: TIDA-01501 Hi,
some Elements are notated with "NC" e.g. C211, C208, C214, R252, C815, C816. These Elements don't also exist in BOM. Are These Elements really disconnected from the System and can be removed?
Thanks, Amr
Part Number: TIDA-01501 Hello,
may you please explain where do the Signals Vp_AUX and Vs_Aux come from? are they from the auxiliary supply TIDA 01503?
Also some other Signals on the schematic are not clear what they exactly are. For example on the schematic…
Part Number: TIDA-01501
Hi,
I'm unable to find the function of Signals BRW, PS_ON, VP_P and ACSNS from the user Manual. Would you please explain their function?
Thank you.
Regards,
Amr
Part Number: TIDA-01501
Hello,
may I ask you please what the current Rating of L4 is? It is intended to use only smd devices. So I will Change it to another part number. May I ask you please which Parameters are must to match so that one achieves the…