Part Number: TIDA-01505 Other Parts Discussed in Thread: TL431-Q1 Hello everyone,
I am currently selecting a flyback converter for a traction inverter emergency supply.
I am happy with the voltage input range of TIDA-01505, but I would like an output…
Part Number: TIDA-01505 Dear Sir or Madam, I would like to get more information regarding the Automotive 40-V to 1-kV input flyback. If possible i would like to have some more details on the constraints of this designe, its efficiency over the wide input…
Part Number: TIDA-01505 Other Parts Discussed in Thread: UCC28C43 Dear TI team,
In Application note TIDA-01505, Input voltage range is 40 V to 1 kV while output voltage range is 15V. My requirement is similar voltage variation but on output side.
Below…
Part Number: TIDA-01505 Other Parts Discussed in Thread: UCC28C56EVM-066 Hi Team,
I am looking for Evaluation Board similar to this design TIDA-01505.
Specification:
Input Voltage= 800V to 1000V
Output power= 15W or 30W
Output Voltage= 16V
For Automotive…
Part Number: TIDA-01505 Other Parts Discussed in Thread: UCC28C43 , UCC12041-Q1 Hi Team,
I am looking for the basic working simulation of IC UCC28C43QDRQ1. Kindly, help me in know more on that.
Thank You
Suma
Part Number: TIDA-01505 In the s chematic of TIDA-01505:
1、Why use Q8(DXT2222A-13) for the UCC28C43QDRQ1? AND does it necessary to use SOT-89 package?
2、When we design a new application. H ow should we design the peripheral parameters of U4(TL431AQDBZRQ1…
Part Number: TIDA-01505 Other Parts Discussed in Thread: UCC28C43 Is the Q15 transistor is necessary to connect in the circuit? If not what negative effect of that parameter Q15?
Part Number: TIDA-01505 I've created a design attempting to following the PSR version of the circuit as closely as I can. But I seem to have run into an issue with the output power limiting itself far earlier then expected. From scope traces I can see…
Part Number: TIDA-01505 Other Parts Discussed in Thread: UCC28C42 , UCC28C43 Hello,
In this reference design, the flyback controller being used is UCC28C43. Due to the part shortage issue, may I ask if I use UCC28C42 instead, shall I modify the circuit…
Part Number: TIDA-01505 As per text above eq. 32, it is mentioned that ," The general rule is to choose the Zener or TVS diode rating to be 1.2 times the reflected voltage: " However the equation below uses
As per "Mitigating Procedure on Voltage…