Part Number: TIDA-01570 Hi,
I am trying to experiment with TIDA-01570 eval board. TI Designs:TIDA-01570.PDF specify to use TI CAN visualizer for this module. Could you please provide teh link for this tool.
Thanks
Part Number: TIDA-01570 Hi,Experts,
when I fllowing the spection(《TI Designs:TIDA-01570》), I have finshed load the xwr16xx_mmw_demo.bin into the FLASH, but I have issues with the test step(Subsection 4),
The CANFD_1 interface J5 , No level fluctuations…
Hi Daniel,
Looks like this thread had been lost in the ocean.
If you still facing the issue, could you first try connect TeraTerm (serial terminal) over the COM port and see the expected output result?
You need to connect both COM ports at required baud…
Part Number: TIDA-01570 Other Parts Discussed in Thread: AWR1642BOOST , UNIFLASH , DCA1000EVM Hi,
I want to collect raw data of TIDA-01570 using DCA1000.
I have connected the LVDS interface and serial port (The TX and RX pin on the J4).
SOP0 and SOP1 has…
Part Number: TIDA-01570 Dear Sir,
Refer TIDA-01570, input power system(LM536253), can pass ISO7637 test?
or have another modify suggestion.
Thanks!
Steven
Part Number: AWR1642BOOST-ODS Other Parts Discussed in Thread: AWR1642 , LP87702 , AWR1642BOOST , MMWAVE-SDK I notice that both these reference designs connect I2C pins of the AWR1642 to the voltage regulator LP87702DRHBRQ1.
As the software for these designs…
Hi
Can TIDA-01570 be connected with mmWave Development Pack and TSW1400EVM to capture the LVDS RAW data?
How about to use the TSW1400EVM SDK to do with it?
I have noticed that it also has a 60-pins connector with the LVDS interface, which is same with AWR1642BOOST…
Part Number: AWR1642BOOST I refer to document TIDUDQ6.pdf – December 2017 which is the reference design document for TIDA 01570.
Please refer to page 18, section 5.3.2
It states that "This design uses Rogers ceramic materials"
However…
Part Number: TIDA-01570 Hello,
The design guide for TIDA-01570 mentions reducing EMI (Section 2.3.2.1.2). I just wanted to know if EMI testing was performed on the board and if the results could be shared.
Thank you,
Faiz
Part Number: TIDA-01570 Other Parts Discussed in Thread: TIDEP-0092 , Hi All,
Q1-When i look "Automotive 77-GHz Radar Module Reference Design With Object Data Output" dacuments figure 20 for Layer Stackup, i understod pcb has 6 layers but at gerber it…