Part Number: TIDA-01573 Hi,
Is it possible to use the low voltage Laser Diode?
I actually want to use sony SD3236VF.
This one is 150mW and operating at 5.3-5.5 V.
You suggest the input voltage within 30-75V, but does it have a chance to use it…
Part Number: TIDA-01573 Other Parts Discussed in Thread: LMG1020 , According to TIDA-01573 app note, in order to really benefit from the high speed capability of the LMG1020 driver, separation of signal ground and power ground is recommended. So the source…
Part Number: TIDA-01573 Hi,
My customer would like to evaluate TIDA-01573 on LMG1020EVM. Could you pls tell me the part number of laser diode which we used to test the TIDA? And, what is the signal generator? Can I use TSW1400 as the signal generator…
Part Number: TIDA-01573 Other Parts Discussed in Thread: LMG1020 Hi,
I am using the TIDA-01573 board. But the measured output rising edge is rather slow. What is the problem? Is the FET damaged? Or my measurement method is wrong?
The 1st pic is Vg…
Part Number: TIDA-01573 Other Parts Discussed in Thread: LMG1020 Dear Sir/Madam,
We are currently working designing a LiDAR system, for this we want to use the reference design of the TIDA-01573. We want to integrate the design in our own system, therefore…
Hi Minseong, The TIDA-01187 and TIDA-01573 were done by two different groups. The two TIDA's are not designed to be compatible with each other. But I think you should be able to replace with TX on TIDA-01187(TSW1400 + DAC5682Z + OPA695) with a pulse gen…
Part Number: TIDA-01573 Other Parts Discussed in Thread: LMG1020 , LMG1020EVM-006 Hi don.
Thank you so much for your suggestion.It took some time to reply so that I barely knew about this and it helped me a lot.
In "TIDA-01573" , Is the maximum output…
Part Number: LMG1020EVM-006 Other Parts Discussed in Thread: TIDA-01573 , , LMG1020
Comparing the schematic from TIDA-01573 - Nanosecond Laser Driver Reference Design for LiDAR (not for sale) with LMG1020EVM-006 - LMG1020 GaN Low-side Driver + GaN FET…
Part Number: TIDA-01573 Other Parts Discussed in Thread: LMG1020EVM-006 , LMG1020
Comparing the schematic from TIDA-01573 - Nanosecond Laser Driver Reference Design for LiDAR (not for sale)
with LMG1020EVM-006 - LMG1020 GaN Low-side Driver + GaN FET…
Hi Jeffrey,
thanks for your answer.Can I understanding your reply in the way below? If the parasitic inductance of a LD is not so small,such as 1nH,and I want to turn off the LD in 2ns at the peak current 50A. I can easily know that a voltage of 25V…