Part Number: TIDA-01590
Dear all,
I have TIDA-01590-E1 board.
If i power ON the board and the board id is shown in my laptop like "Throughput Pheri" then i can able to Pair and connect the device. But the data from the sensor i cant able to read.…
Part Number: TIDA-01590 Other Parts Discussed in Thread: PCA9548A , INA260 , INA229 Hello,
We are looking for the current sense measurement solution for solar plants where voltage string is carry 1500V up to 30A.
This TIDA-01590 reference design seems like…
Hello Carolus,
Can someone from TI, which worked on this reference design TIDA-01590, confirm us what should be creepage/clearance distance for transformer to satisfy 1500 V DC?
Used transformer 750316031 has 11mm min creepage and clearance distance and I…
Hi Guang,
I understand you concern regarding the 600Vdc being present on IN+ of INA195. My circuit use the similar technique as INA260 TIDA-01590 (see below). The INA260 has common mode range of 0-36V on the IN+ and IN- but still sees the 1200Vdc on…
Part Number: INA302 Other Parts Discussed in Thread: TIDA-01590 , INA260 , TIDA-01065
Hi
I am designing 115VAC switch with mosfets(back-to-back configuration) and I want to measure load current with INA302A3. Can I use mosfet’s driver isolated ground in…
Hello AnBer,
Thank you for reaching out on the forum. Could you tell us a little more about your DC DC converter (input, output voltages, and expected current levels, and what general topology are your customer is using). The INA260 shunt is not isolated…
The are many ways to measure current and Texas Instruments has a diverse portfolio to do exactly that!
Here are a few links to get you started measuring current with TI products:
If you don't know where to start with your current measurement design,…