Part Number: TIDA-01615 Can i configure the SPI plus DMA to write the bit banging avoiding to use all the CPU only for the display?
In this way i can use the system not only for the display but also for other activity!
With the DMA i don't have to use…
Part Number: MSP-EXP432P401R Tool/software: Code Composer Studio Hello everyone!
Recently, I want to create a reference design of TI company.
It is called TI design TIDA-01615 10X16 Full-Color RGB LED Matrix Reference Design.
I want to create a display…
Part Number: TIDA-01615 I have followed the procedure:
"Connect the MSP‑EXP432P401R LaunchPad and the LED panel through the BoosterPack connector. Then, plug in the USB wires for the LED panel and the MSP‑EXP432P401R LaunchPad by order. "
Also…
Hi, Martin,
Would you refer to the TIDA-01615?
www.ti.com/.../TIDA-01615
It contains the PCB file for TLC5957RTQ.
Please help to click "Resolve" if the problem is solved.
Thanks.
Regards,
Kenneth
Part Number: TLC5947 Other Parts Discussed in Thread: TLC5957 Hi,
I want to design a 15x15 LED matrix by TLC5947 in Vled 3.3V.
My question is what is the purpose of the zener diode (in TIDA-01615 reference design and TLC5957 datasheet)?
and how to decide…
Part Number: TLC5957 Hello I have to drive 3 dasy chained TLC5957 in a 40x25 RGB matrix. I adaped the code of the "TIDA-01615 Reference Code" to my needs.
The first TLC is working properly as expected, so the 16x25 maxtrix is working. Now I…