Part Number: TPS65983B
Hi Team,
I can't find any materials about TIDA-03027 on ti.com.
How could I get some materials? such as applicable design files (CAD and Gerber files), Test Report, BOM, and schematics.
Thanks very much!
Best regards
Xing
Part Number: TPS65983B
HI Ti,
I'm planning to design the board based on the design of TIDA-03027, and seems like the schematics of TIDA-03027 is no longer available.
Could you suggest any other EVM to replace TIDA-03027? USB 3.0 HUB AND DP OUT(OR…
Part Number: TIDA-03027 Hello Sir/Madam
I wander why design need a buck IC LM3489? Charger can provide almost all voltage and current if 83B DFP negotiate with charger through CC line. LM3489 would lower efficiency of charging system.
Thanks and Best…
Part Number: TIDA-03027 Hello Sir/Madam
TIDA-03027 design can be power by both mobile device and charger. I think charger will power system if there is a charger been attached. If the charger is pull out and mobile device should provide power for system…
Part Number: TIDA-03027 Hi,
I noticed in the TIDA-03027 reference design that the "bus-powered" solution would mean we get a voltage drop through the two load-switches and the buck (efficiency) + inductor.
VBUS on the down-stream facing jacks…
Part Number: TIDA-03027 We are looking to develop a solution that does the following:
There would essentially be two conditions:
Condition/Case 1:
The device is not being charged but has a USB 2.0 device attached. In this case the USB 2.0 device would…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS65983B Hello,
My customer wants to use 2 pcs of TPS65987D to replace the TPS65983B in reference design TIDA-03027 with the updated block diagram as following:
Q1: TPS65983B use UART interface…
Part Number: TIDA-03027 Hello TI E2E.
Is the TIDA-03027 USB Type-C™ and Power Delivery Multiport-Adapter Reference Design available as a development kit? What is the process to get one if it is?
Thanks.
Stephen.
Synaptics
Part Number: TIDA-03027 Hey guys, I'm interested in manufacturing a TIDA-03027 Board (USB-C Multiport Adapter Reference Design) design for early Proof-of-Concept prototyping purposes. For doing so, I downloaded the provided Gerber Files indicated in…
Part Number: TIDA-03027 Hi,
I'm unable to open the Altium CAD files with Atium software, an error message saying " "File name" has invalid format". Am I able to get the files converted to Eagle or another software instead?
Kind…