Part Number: TIDA-03027 Hi,
I am currently making plans to work with the TIDA-03027 reference design as the power adapter design for my project. I just had a couple of questions.
1) I need to step down the 3.3V rail down to the voltage range of 2~2.6V…
Part Number: TIDA-03027 Hi All
The reference design ITDA-03027 is very helpful. After reading it, we some questions about it:
1.The first TPS65983B (U17) ,which is connected with Type-C plug, can only be used as source. The current direction is only from…
Hi ZMMN!
Here is the schematic, which is basically almost identical to TIDA-03027.
Upstream port & TUSB8041
1.Yes USB_VBUS is high. but, 90.9k resistor is replaced with 91k resistor.
2. GRST still has external pullup. I will update as you…
Team,
I need help finding a solution for the following requirements. The initial design was based off of the following TIDA: http://www.ti.com/tool/TIDA-03027#technicaldocuments
UFP plug
Display Port
USB PD, 5V, 3A
Communicates between a smartphone…
Hello,
Here is an example of how you can connect the PD controller to a HUB.
http://www.ti.com/tool/TIDA-03027
It is not necessary, but is recommended that the PD controller indicate that a overcurrent event occurred on its system. This can be done through…
Hello,
None of the TI PD controllers support HDMI alt. mode. We support DP alt. mode. If HDMI is needed, you can use a protocol converter chip like on TIDA-03027
Thank you, Eric
Takisawa-san hello and good evening. I believe you are referring to "Thunderbolt 3", not "Thundervolt 3", correct? If so, perhaps you can start with either the TIDA-03027 or possibly the TIDA-00268 designs. Let me know if this meets what your customer…
Hi,
I am currently making plans to work with the TIDA-03027 reference design as the power adapter design for my project. I just had a couple of questions.
1) I need to step down the 3.3V rail down to the voltage range of 2~2.6V for an LED strip. It was suggested…
Hello Mitchell,
HDMI as an alternate mode is not supported by our Type-C PD controllers as there is no real standard to follow. If you would like to implement an HDMI port, you can follow this reference design ( www.ti.com/.../tida-03027
If you wish to…