Part Number: TIDA-080004 Dear T eam ,
Whenever I operate the DLPC120, it keeps popping up error messages. How can I check and fix this?
=====================.log===========================
Crash File for Automotive Control Program 2.0.0.0 Current Time:…
Part Number: TIDA-080004 Other Parts Discussed in Thread: TMS320F28023 , UNIFLASH HI I am using DLPC 120 Atuomotive Control Program to burn the program for the device:TMS320F28023,my settings are shown here,log following figure shows an error: debugser…
Part Number: TIDA-080004 Other Parts Discussed in Thread: TMS320F28023 , Hi Team,
I ask this from our customer.
Customer is testing the TIDM-080004, by controlling the S9KEAZ128AMLHf, using SPI signal to send commands to TMS320F28023, such as backlight adjustment…
Part Number: TIDA-080004 Hi Expert,
I see in the reference design that "output up to 90 lumens with 7.1-W input power". For the 7.1W power, which point do you calculate? The 12V battery side or 3.3V side? Does the 7.1W power mean the whole AR HUD module…
Hello Andreas,
Welcome to the E2E forums and we hope to assist you with your questions.
You are correct that the DLP3021-Q1 and DLP3020-Q1 are identical except for naming convention.
We use different numbering to distinguish for different applications…
Part Number: TIDA-080004 Hi team,
My customer is designing their prototype referring to TIDA-080004.
The pull up voltage of 3.3V for HDMI HPD signal is regulated on the board, it does not use 5V provided from HDMI source.
Is there any special reason…
Hello,
Do you have access to an oscilloscope? Please go to the following page and you can use the schematic and assembly drawing of the formatter board to help figure out where these test points are.
https://www.ti.com/tool/TIDA-080004#design-product…
Hi,
Are you working with a TI Engineer named Elec Cheng?
We have a similar e2e thread here about the same question.
https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design…
Part Number: DLP2000 Other Parts Discussed in Thread: TIDA-080004 , DLP2010 Hello,
I am planning to use DLP2000 evaluation board for prototyping of my idea which is to get a grey scale video on the windshield of the car or a lens like display typically…
Hello! The DLPC120-Q1 is part of a full chipset. On its own, it is only a controller, designed to format incoming video data to be properly displayed on the DMD. When paired with the DLP3030-Q1 and an LED driver, it can form the electronics portion of…