Part Number: TIDA-080008 Other Parts Discussed in Thread: DLPC900 , , DLP9000
Hi Team
This is a continuation of this Thread
The customer is planning on using TIDA-080008 to replace a RAPCUR era LED projector in order to use new generation LEDs. The projector…
Part Number: TIDA-080008 Other Parts Discussed in Thread: TPS92641 Hi Team,
I have a question that needed clarification for the TIDA-080008 . In the documentation, Table 2 indicates that the max voltage output is configured for is approx 15.8V, then it…
Part Number: TPS92641 Other Parts Discussed in Thread: TIDA-080008 Hi team,
My customer is designing LED driver circuit referring to TIDA-080008, but he cannot find LED Driver Calculator Tool mentioned in the design guide.
Is this tool available?
Best, …
Hi Steven,
Customer RnD concern the current accuracy.
If RnD reference TIDA-080008 reference design, is the current accuracy able to be under 12mA?
Do you have any suggestion to improve the current accuracy?
Best regards,
hi Taito
Sorry I did not find high current application for LM3409. But there is a device TPS92641 that has the same 1A peak current Mosfet drive. It has a reference design for 10A application.
TIDA-080008 reference design | TI.com
Part Number: TPS92641 Other Parts Discussed in Thread: TIDA-01095 , TIDA-080008 Hi,
we have an issue with a TPS92641 LED driver. The schematic is this:
Supply Voltage is 48V, LED String Voltage is 38V, LED Current is 1.5A
We have discovered flicker problems…