Part Number: PCM3168A Other Parts Discussed in Thread: PCM3168 We are the facing issues while integrating pcm3168a codec driver.
Target device and version details as follows:
Kernel version : - 4.19.35
CPU : - i.MX6Q
Based on https://bootlin.com/blog…
Part Number: TIDA-01093 Hello TI technical community,
I was hoping to produce a small number of TIDA-01093 reference boards for preliminary testing, however I was unable to find the drill files necessary to produce the PCBs in the reference design. Is…
Part Number: BQ79616EVM-021 Other Parts Discussed in Thread: USB2ANY
Suggested-;
We do provide reference code with our ARM MCU TMS570. I have already shared the link for getting more details through our Secure Software pages. Please request the same…
Hi again David,
Read some more in your Design Guide, and by " the laser based enclosed optical module" you probably refer to the "laser-based PM sensor" which is used as as a reference during testing??
If this is the case, we probably…
Part Number: BQ25895 Hi
BQ25895 uses a 12V 15W monocrystalline solar panel to charge a single 18650 lithium battery. However, when I use the computer USB port to charge, it shows that the charging is normal.
When the solar panel is plugged in, it cannot…
Hi,
Meet Pandya said: You suggested that a PFC ON switch is required and should be ON afterward once DC is built without boost switching, right?
Yes, you would better turn on the AC power source, wait for stable DC bus voltage, and then turn on the PFC…
Part Number: TAS6584-Q1 Other Parts Discussed in Thread: TIDA-020033 , I notice that on the TIDA-020033 reference design BOM for the reconstruction filters (L100..107) that the value and part number is for 0.47uH.
Is this a typo? Shouldn't they be 4.7uH…