Part Number: CC1120 I have a 434MHZ daughter card that I use on my custom RX and TX boards. In testing with a TRXEB RX board and my custom RX board, I have a TX sending packets from about 3 ft away. Every packet is received every time (in normal mode…
Part Number: CC1120EMK-420-470 Other Parts Discussed in Thread: CC1020 , CC1120 , SMARTRFTRXEBK , , CC1310 Hello TI Community,
I have some "issues" with synchronous serial mode.
Here is the context before my actual question.
I'm currently working…
Thanks for information! I solved the problems. regarding the RSSI, I would like to know the Received signal strength at antenna (RSSI shows the strength at transceiver), for that I try to find the attenuation (loss) between antenna and transceiver (cc1120…
Part Number: CC1120EM-420-470-RD We want to try packet communication between cc1120 and cc1020. First of all, the packet format for cc1020 is unknown. I understand that in order to communicate with the packet, we need to know both the primable and sync…
Other Parts Discussed in Thread: CC1200 , CC1125 Hi,
My customer is evaluating our SubGHz platformsv for a dual-band radio for agricultural applications.
Customer would start with demoboards for CC1200 on the 420-470 MHZ and 868-930MHz bands;
Same for CC1125…
Part Number: CC1120EM-420-470-RD I've ported code to Arduino UNO and that can run Tx/Rx test successfully.
I would like to porting firmware to STM32G071RB board and run the same initial register setting value as Arduino UNO.
after issue STX command…
Part Number: CC1200DK Other Parts Discussed in Thread: CC1200 , , CC1200EMK-420-470 Hello,
Few questions:
Is CC1200 tunable to any frequencies between 420-470MHz?
Are there any parameters in CC1200 transceiver that need calibration over 1-10 years using…
Part Number: TIDC-SIGFOX-CC1120-CC1190-BP Hi,
I am evaluating Ti's Sun-1GHz CC1120-CC1190 boosterPack reference design for sigfox networks. I have modified the boards to make it operate at 868 MHz. So right now I am doing some performance testing with…
Part Number: TIDC-SIGFOX-CC1120-CC1190-BP Hello,
I have a project which is to transmit sensor datas over 10km. For this purpose can use this boosterpack (CC1120-cc1190) with a SMA Antenna? to extend the distance I want to use a sma antenna.
Thank You…