Yes, you can evaluate this using SmartRF Studio 7 : https://www.ti.com/tool/SMARTRFTM-STUDIO
It has a range of output power settings, from +13 dBm to -11 dBm.
Regards,
Zack
Part Number: CC1120 Hi,
we need to design a new system which contains both 434Mhz narrow band (CC1120) and a mesh network based on 868MHz, 27dB PA (CC110x + FEM)
They work on their own antennas (wire or PCB), but async. to each other . The 434Mhz doesn…
Part Number: CC1312R7 Other Parts Discussed in Thread: CC1312R , , CC1310 Hi,
According to my test it looks that the power detector not measuring correctly the RSSI value, on 433MHz band. The reported RSSI value is about 5-6dB higher than the signal itself…
Part Number: CC1101 Team,
1) Looking at the CC1101EMK868-915 kit ( https://www.mouser.fr/new/texas-instruments/ti-cc1101emk868-915-development-kit/ ):
Q:What module is provided in this kit? Is it: http://www.ti.com/tool/CC1101CC1190EMK915 or http://www.ti…
hi Diego P ,
Sorry for the delay in posting the reply.
Diego P said: Have you verified with a spectrum analyzer that the Tx device is transmitting at the configured frequency, 868 MHz based on your register settings?
We don't have Spectrum analyser with us…
Hi,
The default BOM should be for the 915 MHz band if the customer got the board from https://www.ti.com/tool/BOOSTXL-CC1120-90 and has not modified the BOM. We cannot tell from a photograph.
Without setting the IOCG2 and IOCG0 registers the device will…
Part Number: CC1120 Other Parts Discussed in Thread: CC1125
HI,
I want to use the CC1120 to scan from 868 to 878.6Mhz (±192KHz bandwidth) and detect when a message is sent. The messages modulation is (D)BPSK, 100Hz wide, data rate is 100 or 600 bits…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Does cc1120 support interleaving and spread spectrum?If CC1120 confirms that these functions are supported, which registers are involved in configuring these functions?
Hello Nir,
I am closing this thread since this is very old and I assume that this issue has been resolved.
Please create new thread if you are still having trouble.
Regards,
The link opens at my side. Quote from the post " HSM mode on CC1310 refers to 4mbps fixed datarate with 8FSK modulation. It is possible to achieve 1mbps datarate 2(G)FSK and upt0 1.5mbps 4(g)FSK (programmable datarate) on this device as well in the…