Hi Jimmy,
Both of these designs do not implement a complete todays AC Charger.
TIDA-00637 covers most of the system blocks for an AC Charger:
-Pilot signal generation but OPA171 must be replaced by TLV1805 to comply to newer requirements -GFCI with self…
1. for collecting T1-mode meters we recommend to use CC1125 (with 40 MHz XTAL) or CC1310.
An example source code project for a T-mode Data Collector with CC1125 is found in:
www.ti.com/.../TIDC-DSSS868WMBUS-DC
Note 1: that this CC1125 code is NOT the…
Other Parts Discussed in Thread: OPA392 , OPA182 , OPA186 How do Precision Amplifiers fit into my Grid Infrastructure design?
Overview Presentation:
Precision Amplifiers in Grid Infrastructure - Slide Deck
Featuring designs for Rogowski Coils, Multifunction…
Other Parts Discussed in Thread: CC3100 , TIDC-CC3ANTENNA-SELECTION Hello,
We are using CC3100 in our project. regarding power input , in the datasheet preregulated input is mention.
but the input is 1.85V. where as with VBAT it is 3.3V.
The question is…
Hello Nguyen,
Thank you for the information that your design is basically a copy of the TIDC-CC3200SMARTPLUG power supply section. That tells me that the design is already proven and we can concentrate on your physical implementation of it, instead of…
Other Parts Discussed in Thread: CCSTUDIO I am trying to turn our IDE project into a command line build using Nant. I am getting stuck because the makefile is not being generated. The .project, .cproject, and .ccsproject files are in source control and…
Other Parts Discussed in Thread: UNIFLASH CCS constantly returning this error message when entering debug mode on a M35H52C1:
Cortex_M3_0: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
Cortex_M3_0: GEL: File…
Ari,
No, not sure where you are getting that. When using a sensor we use edge based eCAP detection. When using sensorless we use a commutation trigger based on the back EMF voltages. If you want to see examples of this on the F280x you can go to
www…