Hi Sid,
Thanks for your reply.
There are a handful of posts on this forum stating that we can manually import radio configurations from SmartRF Studio, one of them listed below.
https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz…
Hi,
There are basically two scenarios: FHSS or DSSS.
According to FCC 15.247 allows frequency hopping, FHSS (our NB soln) or DSSS (our WB soln):
FHSS : Frequency hopping schemes are often referred to as frequency hopping spread spectrum. To be…
Part Number: BQ51013B Wireless Power Requirements:
-Require 5W
-Active Part Number and industrial temp rated
-Air Gap: 30mm but ideally up to 40mm
-Coil Size: 50mm or smaller is ideal, room to adjust size as needed
-Don’t need to be compliant with any…
Part Number: CC1120 Other Parts Discussed in Thread: CC1310 , Hi,
Could someone please guide me with the CC1120 settings to be compatible with the CC1310 standard LRM?
We have tried to settings some settings using the DSSS PN mode. Only receiving CRC errors…
Part Number: TIDC-SIGFOX-CC1120-CC1190-BP I'm working with this kit . As far as I understand, it's just using LNA_EN, PA_EN, MOSI, MISO, GPIO{0,1,2} and CS_N which are pins: P1.6, P3.2, P2.7, P3.0, 3.1, P2.6, P2.3, P8.1, P7.4 and P2.0
This from…
Part Number: AFE031 Other Parts Discussed in Thread: AFE030 , AFE032 Dear forum: I have a related question here in the specific case of an AFE031 based system. I am sorry if it seems like I am repeating this from a previous thread, but some stuff is still…
Other Parts Discussed in Thread: CC1101 , CC1120 Hello, one quick question... it is possible to use the CC1120 with FHSS in compliance with the FCC 15.247 regulation? it is possible to reach the 1W peak output power? as the max RX filter bandwidth is 200KHz…
We are planning to work on UWB based product design mainly used in industrial plant to track a person.
For which we need your help to understanding the TI based product(compact design) on this domain and provide an intro to understand and conclude on…
Other Parts Discussed in Thread: CC1125 , CC1120 , CC1190 I kindly ask you to give me support to interpret the use of the transceiver CC1120/CC1125 band 869.4-869.650 MHz when it is used in combination with the CC1190 +27 dBm outp. compliant with directive…