Hi Siri, Today I found reference design for multiband Wmbus TIDC-MULTIBAND-WMBUS reference design | TI.com , it says any example code for F-mode Wmbus
Where I can get the example code? I want to use that for my reference to develop Wmbus 433MHz code in CC1312R1…
Part Number: TIDC-WMBUS-868MHZ Hi All,
I want to connect one of my wired MBUS meter directly to Radiocraft RC1180 module.Is it is possible to connect wired mbus meter to radiocraft. If possible please let me know how to connect it.Please let me any…
Other Parts Discussed in Thread: OPA392 , OPA182 , OPA186 How do Precision Amplifiers fit into my Grid Infrastructure design?
Overview Presentation:
Precision Amplifiers in Grid Infrastructure - Slide Deck
Featuring designs for Rogowski Coils, Multifunction…
Cem,
1) I see on the WMBUS page that multiple other TI hardware platforms, including the two-chip solution of the MSP430 + CC112x and CC120x high performance transceivers are also supported, specifically the 868 and 169 MHz bands.
2) A simple example for…
Part Number: CC1120 Other Parts Discussed in Thread: TIDC-MULTIBAND-WMBUS , WMBUS Hi!
I have such settings for Packet RX mode
{CC112X_IOCFG3, 0x01}, // RXFIFO_THR_PKT Associated to the RX FIFO. Asserted when the RX FIFO is filled above
…
Hello Heena,
I would suggest starting in this area of TI.COM
TI Home > Applications > Automotive >Hybrid, Electric & Power Train Systems
www.ti.com/.../overview.page
And this document shows many solutions, including PLC.
Hybrid and Electric…
Hi, thanks for your reply.
1: The board is made by myself ,but it's mostly the similar with TI evm board.
2: The boot log is in attchment.
3: It always tells "time out" no matter whether connect a can slave device or not.
4: It's strange…
Other Parts Discussed in Thread: AM4376 , AM4372 Hi ,
We are Using TI-AM4376 Custom Board and it has 2 Ethernet port when Initialized Hardware with Gel File in CCS PRU-Ethernet ports (Eth-1 and Eth-2 )is detecting ,and when I used to auto boot from Linux…