Part Number: TIDEP-01017 Other Parts Discussed in Thread: TIDEP-01012 , AWR2243 , AWR1243 , TDA2 Dear TIDEP-01017 Team,
I would like to develop a real-time demo on the TIDEP-01012. Cesar from this thread
Is it possible to "install" the TIDEP-01017 Software…
Part Number: TIDEP-01017 Other Parts Discussed in Thread: MMWCAS-DSP-EVM , MMWCAS-RF-EVM Tool/software: Code Composer Studio Hi,
Now I want to acquire adc data, perform FFTs and do some post-processing with the boards MMWCAS-DSP-EVM and MMWCAS-RF-EVM, …
Part Number: TIDEP-01017 Other Parts Discussed in Thread: MMWCAS-DSP-EVM , MMWCAS-RF-EVM
We recently bought a MMWCAS-DSP-EVM & MMWCAS-RF-EVM combination.
When we connected the boards and powered them on, only the Input
12V Power Indicator LED came…
Part Number: TIDEP-01017
Hello,
I run the usecases "cascade_radar_beam_form", and the result is mismatched between GUI and real environment.
I think the reason is calibration of TX and RX.
Can i calibrate the TX and RX just like the usecsaes…
Part Number: TIDEP-01017 Other Parts Discussed in Thread: AWR2243 , Hi,
I'm using TDA2XX for cascade radar development (AWR2243). According to our design, we need a larger memory allocation, but the default in the VSDK is 512M.There are four DDR3 chips…
Part Number: TIDEP-01017 I have the exact same problem as https://e2e.ti.com/support/processors/f/791/t/895057 with the new board that was just mailed to me.
Can someone please let Alec ( AJS214 ) know so he can confirm that this new board also needs to be…
Part Number: TIDEP-01017
In the example of Cascade_radar_beam_form, the following error occurred when modifying the Chirp parameter to set the sample points to 512
[IPU1-0] 14.243518 S: CAPTDRv/SRC/VPSDRV_capturecore.c@line 643:
[IPU1-0] 14.243610…
Part Number: TIDEP-01017 Hi
I modify the sample code of Cascade MIMO object detection of radar sdk 3.8.
And I want to use MUSIC algorithm to calculation the angle of object on DSP1.
Then I need to allocate memory to use SVD.
The size of input data matrix…
Part Number: TIDEP-01017
Hi,
The SDK we applied for MMWAVE-STUDIO-2G was installed with 3.00 version after upgrading, but the manual such as “”mmwave sudio cascade user guide“” is still old (although it is shown written in 2020), so please let me know…