Part Number: TIDM-02000
Hi,
For PCMC Phase shifted full bridge converter, the time period of both active and passive legs should be same.
In the example project of TIDM-02000, there is a difference in time period for both the legs.
For the active leg…
Part Number: TMS320F280039C Other Parts Discussed in Thread: PMP23126 , C2000WARE Hello everyone,
I have a question regarding PCMC control mode. If our DCDC is with very low load. As a result, the input current is also very low, how the PCMC regulation behaves…
Part Number: TIDM-02000
I have two questions to confirm about the peak current mode of TIDM-02000.
The documentation states the following.
"1. Remove resistor R50 from 4-2. The winding current of the secondary side CT is used for average current mode…
Part Number: TIDM-02000
Hello experts
Can somebody help me to figure out this issue happening at the PSFB transformer primary voltage, The issue was occurring in every deadtime.
details -
G1 and G2 are the top & Bottom pwms of first leg. G3 and G4 are…
Part Number: TIDM-02000 Hi,
We are developing a product based on TI reference design TIDM-02000.
The reference design proposes the use of TMS320f28004x with SDK support to implement digital control algorithms. The MCU used in the reference design has lesser…
Part Number: TIDM-02000 Other Parts Discussed in Thread: CONTROLSUITE Hi Team,
In the snap shot above, is the voltage sense filled in the actual output voltage of the system or the maximum sampled voltage ?
And cannot find the calculation.xlsx .
--
Thanks…
Part Number: TMDSCNCD280039C Other Parts Discussed in Thread: PMP23126 , TIDM-02000 , , C2000WARE Hi,
One of my customers is looking at our reference designs PMP23126 and TIDM-02000. But their target MCU is F280039C. Could the TMDSCNCD280039C be used on those…
Part Number: TIDM-02000 We would like to create a reference design for TIDM-02000.
However, I cannot open the schematic (Schematic Editor)and
netlist(PCB Editor) files in KiCAD.
I would like to know how to solve this problem.
The KiCAD bashon is KiCad…
Yale Li 李耀先 said: Is this use for change the SR mode conveniently during the run time? If my customer has already determined which SR mode to use, can this part of the program be placed in the PWM setting of the main function?
Yes, if the customer is not…