Part Number: TMS320F28388D Other Parts Discussed in Thread: TIDM-02011 I have Controller (TMS320F28388D). I Plan to live firmware update without device reset on F2838x( TMS320F28388D ) MCUs via SPI. For this, please provide a reference document or application…
Hi Manish,
We have the Live Firmware Update (LFU) TIDM-02011 reference design that should be able to provide you with the example code.
For more information, please take a look at these application notes:
https://www.ti.com/lit/pdf/spruiu8 (LFU…
Part Number: TMS320F280049 Other Parts Discussed in Thread: TIDM-02011 Hi all,
My customer needs urgent support on this issue. They found that the global/static variables are not initialized after LFU.
They called _c_int00 after LFU, but the variables…
Hi Diao,
Thank you for the detailed question. This is a nuanced topic but I will attempt address each of your questions below.
Short Answer to the Core Question (Q10)
Yes, your understanding is correct. A software-only static library cannot provide…
Prashant,
We have a reference design for this, called Live Firmware Update - using F28003x which contains multiple Flash banks.
The design is TIDM-02011 in the DigitalPowerSDK.
https://www.ti.com/tool/C2000WARE-DIGITALPOWER-SDK
There's a corresponding…
Hang,
Yes, alternate versions will use alternate linker cmd files, this is understood. But there is no additional relationship between the "exact version name" and the linker cmd file. As long as the alternate versioning relationship is maintained with…
Part Number: TMS320F280049C Other Parts Discussed in Thread: LAUNCHXL-F280049C , C2000WARE , TIDM-02011 Tool/software: Hi,
I wanted to perform Live firmware upgrade and referring SPRUIU8a, following the steps as mentioned in 6.2.
Hardware Used: LAUNCHXL…
Part Number: TMS320F28384D Other Parts Discussed in Thread: C2000WARE-DIGITALPOWER-SDK , TIDM-02011 , C2000WARE Hi Team,
Do we have any example of OTA FW update via CAN ?
If no, any plans to provide it ?
Regards,
Geoffrey
Part Number: TMS320F28027 Other Parts Discussed in Thread: TIDM-02011 Hi Champ,
I am asking for my customer. They are still using F28027 and looking forward to doing LFU through I2C.
The method of LFU with reset/without reset has been implemented…
Part Number: TMS320F28386S Other Parts Discussed in Thread: C2000WARE , TIDM-02011 Hi,
I am trying to develop a project which will have:
1. A customer/secondary flash bootloader which is located in flash sectors 0 & 1, on the core CPU1.
2. An application…