Part Number: TIDM-1019 I've purchased an eval board for the MSP430FR6047 Water Meter. I use transducers from Audiowell (same as those used in documention).
The pipe with transducers is on a testing bench with a flowrate (water) fixed at 500L/h.
I read…
Part Number: TIDM-1019 Hi Team, Good day! Need your expertise on our customer's inquiry below: "I have a question about ADC capturing of TIDM-1019. My system's TOF is about 7us and I wanna capture echoes using internal ADC but there is a parameter in…
Part Number: TIDM-1019 Other Parts Discussed in Thread: EVM430-FR6047 , MSP430FR6047 Hi Eddie,
I) Find in attach the EVM Board PIC, and please send me all updated documents related with it.
II) In http://www.ti.com/tool/evm430-fr6047#technicaldocumen…
Part Number: TIDM-1019 Tool/software: Code Composer Studio Hi.
I use MSP430 MCUs Ultrasonic Sensing Design Center GUI and I can get a Absolute TOF result .
Then I use the function MSP430 MCUs Ultrasonic Sensing Design Center provide to get the headers…
Hi Maxime,
The software release should be in around 2-3 weeks. The software will be available at the link below.
http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/USSSWLib/USSSWLibWater/latest/
Hi Antonio,
The EVM and TIDM-1019 are both showing the same revision A of the schematic. The revision can be seen in the lower right corner of the schematic.
I do see that the title in the EVM product folder shows rev. B. I will get this updated…
Part Number: TIDM-1019 Hi,
I've several questions about the "Manual Calibration"
I'm using the last version of USS (02_20_00_18), and UltrasonicWaterFR604x_02_20_00_08
1)
The following step is still necessary if i want to use "Adv. Calibration…
Hi,
Most of your questions are related to the performance on a final product. Well, for TI, we only provided the MCU part of the final product. Customer can choose their own transducers and pipe for their product. So, the performance can be varies between…
Part Number: TIDM-1019 Hi,
1) Is this a good ADC capture at zero flow rate for following settings?
Transmit frequency :986 kHz
UPS0 to UPS1 gap :500 ms
Gain :6db
Capture duration : 50us
Envelope threshold :20
2) I noticed that I always have some waves…