Part Number: TIDM-02013 Hi,
We are going to launch a order of 10 units of TIDM-02013 and once we receive the boards we would like to safely test them. Is there any way to test the AC/DC (PFC part) and DC/DC (CLLLC part) independently?
For example, for…
Part Number: TPS92314 Hi TI team,
I checked and found that TPS92314 can be used for Constant Current LED driver application. Just wanted to double sure that my reading is correct.
My requirement - Input : 90V-265VAC, Output: 24V @150mA.
Please advise…
Part Number: TIDM-HV-1PH-DCAC Hi team,
If the customer want to change to 800-V DC input, 110-V AC output, is it only required to change the tolerance values of capacitors, IGBTs, etc.? Or is it also required to add an additional DCDC buck to 380V in the…
Part Number: IWR6843ISK This IWR6843ISK EVM is a new one which i just ordered from TI.com on Feb.22 2023. And I test it on Mar. 1st
After set the SOP as attateched image, I install the CP210x_Windows_Drivers( download from https://www.silabs.com/documents…
Part Number: TIDM-02010 I have been taking a careful look at this reference design, my question is about the circuit included in file tidm_02010_ac_relay.SchDoc for the COM serial commnications used in this design, since the hardware seems to be full-duplex…
Part Number: TIDM-1000 Hi team,
Here's an issue from the customer may need your help:
The AC input in datasheet is 400 VL-L 50 Hz, Output 700-V DC Nominal. Is derating possible like input AC 220VL-L 50 Hz, output DC 400V DC Nominal. And can it be…
Hi John,
Thanks for your help!
John_K said: Are you asking whether it is okay to calculate duty based on the previous cycle ADC measurement?
Yes, they are asking this. And there is a time delay in the acquisition? Is there a way to minimize the delay? …
Part Number: TIDM-02008 Hello,
I would like to change the output voltage when operating in "Open Loop (AC Output)" mode. Is there a specific variable I can change in the SW to achieve this?
Part Number: TIDM-TMS570BMS Dear team,
I have a similar issue.
I made the appropriate modifications to the TMS570 board so that it connect to the EM1402EVM board (removing R8 and R9 and connecting them to J4-1/J4-2).
When it came time to launch the bq76PL455_GUI…
Part Number: TIDM-02008 Other Parts Discussed in Thread: TIDM-1007 Dear champs,
I am asking this for our customer.
They are interested in TIDM-1007/02008 for CCM Totem Pole PFC.
It's a challenge how to correctly get the AC zero-crossing at different…