Hi Brian,
The same code that is used to interface the ADS1292R in EVM(ADS1292R Performance Demonstration Kit) is also used in the TIDM-BIOSIGNMONITOR reference Design.
So, Could you please check internally with your colleagues which are worked on this…
Other Parts Discussed in Thread: AFE4403 , ADS1292R , TIDM-BIOSIGNMONITOR , ADS1292 Dear TI E2E™,
We have to make a new design for Heart rate monitor with Pedometer, Memory for Datalogging, Batterie management, and Bluetooth connexion...
This design…
1. I am not sure what evaluation kit you are referring to, however if it is the RF430FRL152HEVM, the design files can be found here : www.ti.com/tool/TIDM-RF430FRLSENSE
2. There are three ADC inputs on this chip. Two of them can be used to measure resistances…
Hi Frank -
A1. The ADS1292ECG-FE actually has 3 segmented ground planes - one for Chassis, one for Analog (the AVSS node) and one for Digital. These are all tied together by zero ohm resistors. The performance of the board is good, so there should…
Joohee Kim88 said: First, my sensor is very small, so the nfc chip should be small. Can I possibly get a bare die for the RF430FRL152H ?
We don't have bare die available for production at this time. I will check internally if we have any samples.
…
Part Number: ADS1291 Other Parts Discussed in Thread: ADS1292R
hi:
I now use the nordic nrf52832 to debug the ADS1291. Now the problem is that the acquired signal has no QRS waveform. The waveforms drawn by the schematics and acquired data through matlab…
Hi Tan, Thanks for supporting our ADS1291! We realize the EVM firmware is a bit outdated. For now, the only other example code that I can recommend was written by our MSP430 team for their Bio-Signal Monitor Reference Design, which also features our…