Hi Hang,
Appreciate you clarifying the requirements. Can you clarify a few more items:
- Do they need DFU without POR?
- Is DFU with a reset acceptable e.g. like a Watchdog reset? If yes, we have an example for that in the TIDM-02011 F28003x Flash kernel…
Target Application: Automotive Energy Management Products
MCALs required : We are using following Peripherals from sysconfig >> DIO, ePWM, ADC, CPU Timer, Watchdog, MemCfg, MCAN, PCAN, DAC, SPI, I2C, ECAP, FSI, CLA.
Hi Jonathan,
I try the code below that should similar with yours as below
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// Configure GPIO
P1OUT = 0;
P1DIR = 0xFF;
P2OUT …
Hi OH,
I think that maybe the reason. As EMDC lib is not open source to customer. The best solution would be: https://www.ti.com/tool/TIDM-THDREADING?keyMatch=TIDUB70A . It use this FIR table to handle the different phase shift caused from the current sensor…
Part Number: MSP430AFE253
Hi team,
Here's an issue from the customer may need your help:
This customer wants to design a DC electrical energy power meter, the voltage is 1000V, and the current is tentatively 1000A. The voltage adopts a voltage divider…
Part Number: TIDM-02012 Other Parts Discussed in Thread: SYSCONFIG Dear Forum,
I am trying to get the TIDM-02012 eCompressor example running with a custiom motor.
I have a multitude of problems:
With the example from SD 4.01 I manage to run my hardware…
Part Number: TMS320F280049C Other Parts Discussed in Thread: C2000WARE , TIDM-02011 Hi all,
As the title mentioned, the scenario is described below.
Compiler Version: TI v22.6.0.LTS
C2000WARE 4.3.0.00
The boot-loader code based on flashapi_ex2_sciKernel…
Part Number: TIDM-02009 Other Parts Discussed in Thread: TIDM-02000 Hi,
I'm investigating the modes of operation of SR at PSFB CDR topology.
I saw that TI implemented different SR modes.
Mode 0 as no SR's are driven. SRs are only driven at diagonal…
Hi Yale,
Yale Li 李耀先 said: In the three-phase three-wire Vienna rectifier , how does the circled place in the figure play the role of the neutral line?
This is explained in the user guide:
"Figure 3 shows a simplified, single-phase diagram of the Vienna…
Part Number: DRA829V Other Parts Discussed in Thread: DRA829 , TDA4VM HI I am analyzing on DRA829V Processor for my new product design & development. Could you help me getting answers for this below questions from Technical Team?
Note: Planning to use…