Part Number: MSP430I2041 Other Parts Discussed in Thread: TIDM-TWOPHASEMETER-I2040 , TIDM-SERVER-PWR-MON Support,
I'm using the TIDM-SERVER-PWRMON kit and SW.
1. Verify that readings are updated every 4 AC cycles? Where in the code is this set? Can…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: TIDM-TM4C129POEAUDIO , , TPA3111D1 , OPA322 For our NVR project we need to make two separate Audio Boxes that will be connected with NVR over ethernet. This Box should be able to provide two way…
Hi
So far, I can't find the direct information on metrology formulas
Three-Phase Metrology With Enhanced ESD Protection and Tamper Detection Reference Design (TIDM-3PHMTR-TAMP-ESD) should be the reference.
The previous E2E thread discussion is the reference…
Part Number: TIDA-00299 Other Parts Discussed in Thread: AMIC110
I am new to EtherCAT and assessing it for a potential application. In my current application, I am controlling a SPI device from a Host PC via an FTDI USB bridge device. Each burst of SPI…
Hi Eason,
Sorry for late reply.
Thank you for the information. I am still in the process of confirming the information I received, but please let me ask question.
Eason Zhou said: Q4:Does EVM perform calculations assuming a Y connection or a Δ connection…
Part Number: TIDM-TMS570BMS
I made the changes as per your suggestions, but how do I check that my NHET is working properly. Also , Even now when I connect the TMS570 to the host PC, the BQ76PL455a GUI still shows "the COMP port cannot open". Please guide…
Part Number: MSP432E401Y I'm currently designing a microcontroller board with MSP432E401Y which uses EPI Host bus muxed mode for interfacing with 3 devices(SRAM, Parallel Flash and FPGA)
To segregate the address and data line, should i add a D-latch…
Part Number: TIDM-2PHASE-SUBMTR-FW2 Other Parts Discussed in Thread: MSP-ISO
The Two Phase Embedded Metering Firmware Upgrade reference design shows the communication of multiple devices performed over I2C and finally connected to host using a I2C to RS232…
Ercan,
*Note that TIDM-1005 has been obsolete since 2021, so there is no longer any direct hosting or support of the reference design. However, I would be happy to help you out from my own understanding and knowledge of the solution.
You might be referring…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: TIDM-02005 Dear person in charge
I have a question on "TIDM-02005_Design Guide Optimized Ultrasonic Sensing Metrology Reference".
In the process of calculating absoluteTOF, it is stated…