Part Number: TIDM-SOLARUINV I would like to ask for TIDM-SOLARUINV reference design, there are two different type of current sensor used.
One is shunt-based which is used at DC-DC converter side that interfaces to PV module and the other is Hall current…
Part Number: TIDM-SOLARUINV Other Parts Discussed in Thread: UCC27324 Hi, I was referring to the gate drivers in the reference design and I came across these two designs:
Full Bridge Gate Driver (p. 3, highlight mine):
I assume the highlighted Zener diodes…
Part Number: TIDM-SOLARUINV Hello team,
Customer is evaluating TIDM-SOLARUINV board.
We would like to have further clarifications on the utilization at 220V 50Hz output.
Are there any changes needed?
How was it evaluated at 220V?
Thanks and best regards…
Part Number: TIDM-SOLARUINV Hi Team,
Customer is looking for a bidirectional converter from AC 230 V to DC 380 V and the other way around. Below is the customer details.
" We have a DC-microgrid that needs to be connected to the AC-grid. I was wondering…
There is one for flyback based but not interleaved - TIDM-SOLARUINV reference design | TI.com and another based on interleaved boost + LLC - TMDSHVMPPTKIT Development kit | TI.com
Part Number: SM72295 Other Parts Discussed in Thread: TIDM-SOLARUINV Hai, I am using SM72295MA IC for gate driver for the flyback converter of solar microinverter, which is same as the TI micronverter reference design. I am not able to get output from…
Part Number: TIDM-SOLARUINV Hello,
I am checking this reference design of TIDM-SOLARUINV and trying to simulate a design for specification changes.
In this design, I am taking two considerations. The first one is using MOSFET,transformer, clamp capacitor…
Part Number: TIDM-SOLARUINV Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC Hi there, I am building a bidirectional grid-tied power supply/sink and came across the TIDM-SOLARUINV. I see that the design calls for diodes in the flyback converter, but…
Part Number: TIDM-SOLARUINV hello
i want to make solar charge controller with offline inverter ,
inverter rating
input - 12/24VDC
output - 230VAC
inverter rating - 300-400VA
please suggest me if i add MPPT/PWM charge controller with " Digitally…
Part Number: TIDM-SOLARUINV When a DC voltage supply is connected to the PV input via JP3 and TP13, the board appears to have a short circuit at the input. Applying an input voltage draws a large amount of current; when 0.5 V was provided, the board drew…