Part Number: TIDM-TM4C129XNFC Tool/software: TI-RTOS Hello
When my code size in the flash passes 720K (0xB0000 bytes) the code can run only from debugger, but not after restart.
my .cmd file looks like this:
/ * The starting address of the application…
Part Number: TIDM-TM4C129XNFC I’m following www.ti.com/.../tiduag2a.pdf to get the TIDM-TM4C129XNFC sample code up and running.
Page 19 of tiduag2a.pdf instructs me to program the CC3100 using the CC31XXEMUBOOST board and mentions that the HTML…
Part Number: TIDM-TM4C129XNFC Tool/software: TI C/C++ Compiler Hi,
I'm trying to get the http://www.ti.com/tool/TIDM-TM4C129XNFC
Once I switch from TI-RTOS 2.14 to 2.16, I get the following errors. I guessed some functionality has moved into the framework…
Part Number: CC3100BOOST Other Parts Discussed in Thread: CC3100 , CC3100SDK Hi,
I’m trying to get the TIDM-TM4C129XNFC referenced design working, so recently purchased all the hardware it requires.
I’ve since been told that this reference design used…
Part Number: TIDM-TM4C129XNFC Tool/software: TI-RTOS Hi,
I need to read ISO14443A/B Type 4 NFC cards, so I’m using:
This setup: www.ti.com/.../TIDM-TM4C129XNFC
These instructions: www.ti.com/.../tiduag2a.pdf
To support this software I have…
Other Parts Discussed in Thread: EK-TM4C1294XL , CC3100 , TRF7970A Hello,
I'm modifying the TIDM-TM4C129XNFC example to run on my EK-TM4C1294XL. I removed the sections of the code that run the CC3100, and instead have melded this example with a USB bulk…
Other Parts Discussed in Thread: EK-TM4C1294XL , CC3100 , TRF7970A (Note: This is a crosspost from the RFID forum, where I was informed I might have better luck posting this question on these forums)
Hello,
I'm modifying the TIDM-TM4C129XNFC example to run…
Hello Neeraj,
Neeraj Hebbar said:
Will dlp7970 will work with cc3200sf-launchxl
With the same NFC tool?
In theory but you would need to do a lot of software porting and that would be very complicated. It is not a solution we offer much support for beyond…
Hello Stephen,
TI has our own NFC/RFID reader/writer devices, as such as we will not offer support for an NXP solution.
If you want to read NFC/RFID tags, look into our TI design: www.ti.com/.../TIDM-TM4C129XNFC
Hello Vamsi,
Unfortunately we don't have any RTOS experts on the team, so this is not a query we can support in detail.
I would recommend reviewing the TI-RTOS handling of this TI Design to see how the NFC communication was dealt with: www.ti.com…