Part Number: TIOL111 Hello,
My customer has a question for TIOL111. In their system, L+ is not powered for a long time while VCC_IN is powered. Is this condition no problem?
Retgards, Oba
Part Number: TIOL111 Other Parts Discussed in Thread: TIOL112 Hi,
I am debugging a custom board with TIOL111 on it. TIOL111 can limit the current to the communication C/Q pin by inserting a resistor Rset between the 6th pin ILIM_ADJ pin and GND.
Looking…
Part Number: TIOL111 Other Parts Discussed in Thread: TIOL112 , Hi Team,
the datasheets of the TIOL 111 and TIOL112 specify an integrated EMC protection against "±1.2 kV/ 500 Ω IEC 61000-4-5 surge".
However, my copy of 61000-4-5 as well…
Part Number: TIOL111 Hello,
I am using TIOL111 (without an internal LDO) part in my design. 3.3V Input for TIOL chip is generated externally by DC/DC buck converter IC (LMR14010) with input +24V.
Application : I am driving 50 numbers of LEDs with the…
Part Number: TIOL112 Other Parts Discussed in Thread: TIOL111 , Hello,
I want to confirm if there is any difference in reverse polarity function between TIOL111 and TIOL112.
While the TIOL111 datasheet says “Reverse Polarity Protection of up to 60 V on…
Part Number: TIOL111 Other Parts Discussed in Thread: TIOL112 Hello,
My customer would like to know MIN and MAX value for IO_LIM with 20Kohm R_SET. According to Figure4 in the datasheet, TYP value is around 170mA. I understand that we don't have guarantee…
Part Number: TIOL111 Other Parts Discussed in Thread: , , TIOL112 , LM5160 We are having issues where the transceiver is behaving strangely over time. Below is the relevant schematic. Our device is not responding to the IOLink master wake-up request - we…
Part Number: TIOL111 Hello,
Have you seen a customer add any type of security or encryption to an IO Link interface? My customer is looking to authenticate devices that plug into a console. IO link looks to be a good fit with the exception that they want…
Part Number: TIOL111 Hello Team,
the TIOL111 without LDO has a need on Vcc_IN for a capacitor of 1uF.
Where that need comes from?
Is it needed for normal operation (internal circuitry voltage stability) or for system surge test/EFT test?
Thanks,
SunS…
Part Number: TIOL111 Hi Team,
When we use TIOL111DMWT in our design we are able to see 1V in 3V3 Plane when we give 24V alone and 1V in 24V plane when we give 3V3 alone.
What are the causes for such issue? and solution for such issue?
CAD is carried out…