Part Number: TIPD164 Other Parts Discussed in Thread: INA826 , ADS1248 , , INA159 , INA823 In TIPD164 design, they have used INA826 and INA159 for converting voltage and current source to required range for ADS1248 IC . Why cant we use INA826 directly using…
Part Number: TIPD164 Other Parts Discussed in Thread: ADS1248 Dear TI's experts,
i cannot get the results of the Offset (mV) shown Table 6-8 ( https://www.ti.com/lit/ug/tidu491/tidu491.pdf?ts=1630943856512&ref_url=https%253A%252F%252Fwww.ti.com%252Fsolution…
Part Number: TIPD164 Hello,
I planing to use TIPD164 Analog Input Module for Industrial Outputs and Temperature Sensors module.
But I realized your module is obsolete. I want to know why your module is obsolete. If the card have a trouble then can you…
Hello Ivan,
As you have mentioned, at the input, the XTR105 is intended for a 2-wire RTD or 3-wire RTD probe/sensor. From the output perspective, the XTR105 is a two-wire current transmitter, producing a 4-20mA current output.
Unfortunately, we do not…
Hi Nandha,
Thanks for sharing further inputs.
I see that the MCU is on the left side of isolator sitting on system ground labelled C_GND. The outputs of digital isolator and RS-485 are all on the isolated ground labelled ISO_GND on the isolated side…
Hi Purvik,
You should search our library of reference designs for help with this request. Two designs that come to mind that can help you are:
https://www.ti.com/tool/TIDA-00550
https://www.ti.com/tool/TIPD164
The first link uses the ADS1262, but accepts…
Hi Kai,
We have short tech doc on using the ADS125H02 for +/- 10V measurements here: http://www.ti.com/lit/an/sbaa387/sbaa387.pdf
For current measurements, we don't have any reference designs specific to the ADS125H02, but we do have some reference designs…
Hello Zeeshan
Need for group isolation will simplify the design.
The switch and the interface can be controlled using digital isolators.
Please refer the below and note that we may not have solutions exactly matching your requirement.
TIDA-00118
TIDA-…
Hi Shreyas,
No, you do not have to use all 16 ADC channels on the ADS1158. You can either select the two channels you want to use and allow the auto-scan sequencer to multiplex (ping-pong) between these two channels, or you can use the fixed-channel mode…