Part Number: TL064 Hi team,
The following changes in the data sheet are not reflected in the tables in the data sheet. "Changed typical input voltage noise density at 1 kHz from 42 nV/√Hz to 30 nV/√Hz." Which is correct?
Thanks, Ryu…
Part Number: TL064 Hi,
All TL06x parts have the same datasheet, so I'm looking for the difference between all TL064 variants. Is there a table showing all the differences?
Thanks,
Ye-Sheng
Part Number: TL064 Hi team,
We found that there are M and Q series of TL064. May I ask whether these two series have the part number which have the same package? Are these two new series? Since there are TBD words in the selection table. Are there samples…
Part Number: TL064 Hello, I would like to ask you for help. I have basic voltage follower taking signal from voltage divider. Issue is that if on the input is voltage lover than 1 V, on OUTPUT is + 5V. If voltage on input is higher than 1 V amplifier…
Part Number: TL064 Hello,
I'm re-implementing a design revolving around a TL064 from STMicro but would like to do it with the TI part instead. Are there any differences between the TI and ST parts that would make them incompatible?
Thanks!
-Ted …
Part Number: TL064 Other Parts Discussed in Thread: OPA2990 A Question from one of my customers:
"If we operate a TL064 opamp from a single ended 21.6 volt supply. How close can we take the inputs to ground?"
We don't specify the TL064 for…
Hello Surya,
I have looked around online and could not find a TL0641. But as Clemens mentioned, the TL064 spice model is on the product page under the design and development tab.
https://www.ti.com/product/TL064#design-development
As Clemens mentioned…
Part Number: TL064 Other Parts Discussed in Thread: TINA-TI , TL072 Hi,
The symptom that input signal is gained in spite of the voltage follower occurs as below attached.
This situation occurs on the below situation;
V+=5.231V, V-=-4.959V, Input signal…
Part Number: TL064 Hi,
I would like to know the value of Isink and Isource of TL 064.
What is the minimun value of Isink and Isource?
Best regards, Seishin