Part Number: TL082-Q1 Other Parts Discussed in Thread: TL082 , OPA627 , TLV9352 , TLV9352-Q1 Hi everyone,
As shown in the figure below, an abnormal phenomenon was discovered when the Inverting Amplifier Circuit was observed.
I want to know what the solution…
Part Number: TL082-Q1 Other Parts Discussed in Thread: TINA-TI , TL082 Dear team,
Please help check if there were any stability issues based on below schematic provided by customer.C143=2.2uF
Do we also have internal block schematic simulation model…
Part Number: TL082-Q1 Other Parts Discussed in Thread: LM358B Hi all,
My customer is experiencing an issue where the oscilloscope test on the -VIN end of TL082-Q1 has an interfering waveform, the -VIN end test on the LM358B does not, and the solution…
Part Number: TL082-Q1 Other Parts Discussed in Thread: TL082 Hi team,
Hope you have a good day.
My customer is using TL082IDRQ1, and have test the case temperature is 95°. This part operating temp is 85°.
Since they didn't find the thermal information…
Part Number: TL082-Q1 Hi all,
The VCOM output waveform was dropped and the voltage drop improved with the VOUT foot plus 10K pull-down resistor, what is the principle?
thanks
Part Number: TL082-Q1 Other Parts Discussed in Thread: TL084 , TL082 We purchased the device through mouser on September 2, 2019. Brand: Ti model: tl082qdrq1 quantity: 250pcs Batch: 1804.
The output waveform of the chip is as follows: the peak duration of…
Part Number: TL082-Q1 Other Parts Discussed in Thread: TL3472-Q1 Hello,
TL082-Q1 has minimum slew rate specification as 8V/us. Is this for rising and falling slew rate? TL3472-Q1 has rising and falling slew rate specifications. If this is only rising slew…
Part Number: TL082-Q1 Hello,
Could you please let me know the slew rate variation of the following conditions? 1. Slew rate vs. Vcc+=10V to 16V, Vcc-=0V 2. Slew rate vs. temperature (Ta=-40C to +125C)
Best Regards, Ryuji