Part Number: TL1431-SP Hi For the reference input voltage there is a minimum value of 2.46V and a maximum value of 2.55V stated in the datasheet. On the first page is a initial tolerance of 0.4% stated which is less than the previously stated value. Can…
Part Number: TL1431-SP The reference input current is listed as 1.5 to 5uA over full temperature range. The deviation over full temperature is 3 uA. Do you have information as to how these vary with temperature to determine these values with a restricted…
Part Number: TL1431-SP Do we have any characterization or limits of the Vref variation due to aging on this device?
Would it just be contained in the electrical specs in section 6.5 of the datasheet?
Part Number: TL1431-SP Hi Team,
Can you please support with dummy packages of following devices?
List of ICs used
Package
TL1431-SP
U0010A
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: TL1431-SP Hello, we need single event latchup data (SEL) for the 5962R9962001VHA (TL1431MDREP ). Is that something TI can provide??
THanks, Adam
Part Number: TL1431-SP Hello,
Why the Vref voltage max @25°C is given at 2.54V in your datasheet ( SLVSB44C) and at 2.525V in the SMD ( 5962-99620) ? Which value is correct ?
Regards
Nicolas
Part Number: TL1431-SP Other Parts Discussed in Thread: TL1431 , , TL431 Question about using the TL1431 as a delay circuit in the comparator mode. This would be open loop mode with a resistor to the ref pin and capacitor to ground. The ref input through…