Part Number: TL1963A-Q1 Hi team,
my customer is seeking the 12V to 5V/2A version LDO, is there any recommendation?
please let us know if there are any suggestions, automotive version is not a MUST.
Best regards
Fanbin
Part Number: TL1963A-Q1
Hi support team, Why are the RθJA of TL1963AQKTTRQ1 and TL1963AKTTR different?
TL1963AQKTTRQ1 RθJA=22.8℃/W TL1963AKTTR RθJA=32.9℃/W
Regards, Dice-K
Part Number: TL1963A-Q1 Hi Team, Do we have information on the maximum dimensions of the TL1963AQKTTRQ1 thermal pad? Unfortunately only the minimum dimensions were specified (Highlighted below). Thanks in advance! Kind Regards, Jejomar
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TLV767-Q1 Hi team,
We have design in TL1963-Q1 replacing OnSemi NCV57152DSADJR4G. From datasheet description, the operation temperature range is up to 125C. However, in the abs max rating table the…
Part Number: TL1963A-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have LDO that can support following spec?
SPE :
1.Vin=16V
2.Vo=8V
3.Io_max=1A
4.IC temperature is less than 100 degrees when Io_max
>>> TL1963A-Q1…
Part Number: LM1117 Other Parts Discussed in Thread: LP5912 , TPS709 , TPS7B7701-Q1 , TPS7B4256-Q1 , TL1963A , TPS7A45 , TPS706 Hi team,
Does TI have some feature like this? the integrated back-to-back diode of LDO?
Like the below block. SGM2205.
Due to customer…
Part Number: TPS7A26 Other Parts Discussed in Thread: TPS73801 , TL1963A-Q1 Hello TI,
I am using TPS7A26 to generate 5V outptut voltage with 2% tolerance from 8.5V input voltage and the load current required is 100mA. I would like to protect output of this…
Part Number: TL1963A-Q1 Hi Team,
A customer is using multiple TL1963-Q1 LDO regulators in their applications and would like to know more details about the Thermal Overload Protection of this device. Here are the information that he would like to request…
Part Number: TL1963A-Q1 Good day.
Our customer would like to know the die power dissipation for TL1963AQKTTRQ1. In section 10.3 of the datasheet, there was an equation and computation for the power dissipated by the device. Is the 1.41 W the same with the…
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TL1963A What is ramp-up time of this LDO?
What is the delay time between shut-down pin to output voltage?