Part Number: TL4242-Q1 Other Parts Discussed in Thread: TPS92613-Q1
Hi,
Customer is using TL4242-Q1 for TAIL (Fender/Trunk) project.
Spec :
- LED : 1EA (0.7W SUPER RED LED)
- LED current: 125~185mA
- Input Voltage : 9~16V
* DELETE Schematic
1. Please…
Part Number: TL4242-Q1 Other Parts Discussed in Thread: TPS92613-Q1 , , TPS92610-Q1 , TPS92611-Q1 , TPS92612-Q1 Dear all,
Is there any alternative solution for TL4242TDRJRQ1?
Proposing P2P device would be perfect, but any comments on the device that has similar…
Part Number: TL4242-Q1 Other Parts Discussed in Thread: TL4242 , TPS92611-Q1 , TPS92613-Q1 Hello, I intend to use the TL4242Q1 in a new product, as I never used it before I need to make sure the design is correct.
The product is a tail lamp used in a vehicle…
Part Number: TL4242-Q1 Hi team,
Customer need to evaluate which thermal performance is better between TL4242QKTTRQ1 and Infineon TLE4242G ,
Do you have the thermal resistance comparison between TL4242QKTTRQ1 and Infineon TLE4242G? Or any comment for this? …
Part Number: TL4242-Q1 The datasheet says the current setting equation applies between 0.39 and 10R, but doesn't specify a minimum output current. I would like to use this part to run a string of LEDs at 35mA, which requires a 22R reference resistor …
Part Number: TL4242-Q1 Other Parts Discussed in Thread: TPS92610-Q1 , , TL4242 Actually i need spice model for TL4242-Q1 and TPS92610-Q1. I am using Micro Cap 11 Simulation Tool.
I try to contact via your site but i can't. Finally i get this route - contact…
Part Number: TL4242-Q1 Is the behaviour of the part predicatble with PWM input voltages between the maximum low and minimum high voltages? I would like a simple, low-cost method for shutting off the light when the temperature hits a maximum specified…
Part Number: TL4242-Q1 Are there any STEP files available for the above part in the WSON package? I've tried my usual sources for such things, but can't find it under the part number or the package name.
Part Number: TL4242-Q1 Other Parts Discussed in Thread: LM3402 , TL4242 Hi there,
Since TL4242-Q1 is a current-controlled regulator, I'm wondering how the output voltage is determined?
In another current-controlled device LM3402, I found a description…