Part Number: TLC2254ATLC2254AIDR This model has two kinds of screen printing, one is with LOGO, the other is without logo, are both kinds of screen printing normal, please confirm
Part Number: TLC2254A Hello,
If I am reading the datasheet properly then the max input voltage if powering for 3.3V would be 1.8V? What happens when that is exceeded?
Thanks, Lindsey
Other Parts Discussed in Thread: TLC2254A , TLC2254 Hello,
We are using a TLC2254A Op Amp in a single supply circuit. The spec indicates:
supply voltage, VDD+ as 8V
supply voltage, VDD- as -8V
Diff input voltage as +/-16V
input voltage, VI (any input)…