Part Number: TLC549 Hi team,
Customer need to find a alternative 8bit SAR ADC to replace the EOL part TLC549.
For pin to pin selection, I found TLC1549 but it's 10bit ADC which is higher too much than TLC549.
For non pin-to-pin part, I found TLV0831…
Part Number: TLC1549 Dears,
Customer is using our TLC549, but this device is EOL, they are going to switch to P2P device TLC1549.
Can you please confirm if they need do any change on driver software when switch TLC549 to P2P device TLC1549?
Thanks and…
Part Number: TLC1549 Hi team,
My customer want to replace TLC549 with TLC1549, but they meet problem with ADC driver code, the code they modified from TLC549 driver always read back wrong result.
Can we provide C code for TLC1549 driver? Thank you!
…
Hello,
The slave select is handled via the GPIOs and register settings in USICTL0 register. Here is an example of a microcontroller interfacing with a TLC549 8 bit ADC via SPI interface:
int main ( void )
{
WDTCTL = WDTPW + WDTHOLD;
// Stop watchdog timer …
Other Parts Discussed in Thread: MSP430F2471 , CC2500 , CC1101 Hi All,
I'm trying to interface an msp430f2471 with a CC2500 using the SPI mode through USCI_B0 ports.
I've found this example from TI:
int main(void) { char data;
WDTCTL = WDTPW + WDTHOLD;…
Yeah! There are many!
Are you using CCS5? You can get examples in the TI resource explorer.
This is the sample code msp430g2xx2_usi_05, for example ;)
#include <msp430g2452.h> void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer P1OUT…
Kevin,
From the MSP430 LaunchPad Wiki page , you can download the MSP430G2xx1 Code Examples zip file slac463a.zip that contains several USI examples for SPI
mode.
i.e. msp430g2x21_usi_02.c SPI full-Duplex 3-wire Master msp430g2x21_usi_03.c SPI full…
To follow up on the above post, although we don't have a software SPI app note, we do have the following code example:
//****************************************************************************** // MSP430x11x1 Demo - Software SPI Interface TLC549…