Part Number: TLC5916-Q1 Hi team,
My customer consider to use TLC5916-Q1 for their project. However in datasheet JA thermal resistance, it is quite high for them and can't accept it.
On the other hand, there are several information about JA thermal resistance…
Part Number: TLC5916 Other Parts Discussed in Thread: LP5861 Customer is looking for a 15ch brightness control for LED driver. the PWM dimming is 1KHz.
Is there device that is able to support individual current control per channel? It means that the each…
Part Number: TLC5916 I am looking to decipher the date code marking on TLC5916IPWR LED driver IC's.
The IC top markings are:
Y5916 99K G4 C3Y1
and
Y5916 84K G4 CNR0
Any help assistance would be greatly appreciated.
Part Number: TLC5916 Other Parts Discussed in Thread: TPS92390 , TPS61196 Dear experts,
Customer is finding 4 channel current sink solution, their current requirement is 100mA/channel and max LED voltage is 70V (23 LEDs in a string).
The maximum channel…
Part Number: TLC5916 I found TLC5916IPW's competitor, TLC5916IPW-P on Rochester.
But I could not find the datasheet of TLC5916IPW-P.
I guess that TLC5916IPW-P is full compatible with TLC5916IPW, correct?
Is there careful point of replace TLC5916IPW-P…
Part Number: TLC5916 Hello everyone,
i am asking if i can apply PWM signal to my design but i don't see about it in the datasheet, if yes, what is the maximum frequency i can run?
Thanks.
here is the link of the datasheet:
www.ti.com/.../tlc5916…
Part Number: TLC5916 Hello Everyone,
i am using the TLC5916, and i am wondering if i can control the current going through the leds by a digital potentiometer, but as you already know that the digital potentiometer only allows 1 or 2 mA of current to go…
Part Number: INA118 Other Parts Discussed in Thread: LM317 Hello,
I have only one issue i don't no the reason of it, i am connecting the leds with the led driver, the led driver is supplied by a 5 volts voltage regulator "LT323A" ,the 12 volts over the…
Part Number: TLC5916
I know! Why the heck would anyone want to do that?!? But, what if you wanted two brightness levels--levels that extended beyond the dynamic range of the " 256-Step Programmable Global Current Gain " feature?
Well, you might…