Hi Gracie,
Thanks for your continuous support, please clarify one last question.
Q1. //Send DC/BC/FC data thru GS Data Path............ you can find this comment at line no. 104 of the software you have provided. what does GS data path mean, is it sending…
Part Number: TLC6C5716-Q1 Dear expert,
Customer choose 1.5K for resistor for IREF and measured Iout(MAX) is only 10mA.
It doesn't match below curve.
Could you give your comment? Thanks
Part Number: TLC6C5716-Q1 Hi team,
I have two questions.
1. Does the parameter K(out) have temperature characteristics and variations? If you have such data, please share it.
2. What are the guidelines for improving EMI performance? For example, adding…
Part Number: TLC6C5716-Q1 Other Parts Discussed in Thread: TLC6C5712-Q1 Hi Team,
Do we have appropriate solution that can replace PCA9955B? 25mA/ch is ok, but it needs I2C control.
Regards,
Roy
Part Number: TLC6C5716-Q1 Other Parts Discussed in Thread: TLC5916-Q1 Dear expert,
How to estimate TLC6C5716-Q1 power dissipation?
For example, VCC=3.3V, LED current= 10mA, LED supply = 5V, LED voltage = 3V (5-3=2V is burn in TLC6C5716-Q1 , right?)
10…
Part Number: TLC6C5716-Q1 Hi team,
Could you advise whether it is possible NOT to use Latch pin?
If Latch pin is unused, should it be left floating or tied to GND?
regards.
Part Number: TLC6C5716-Q1 dear team,
I'm trying to use TLC6C5716-Q1 to control 4 rgb led ,can you provide a sample code ? because I found it's hard to control it.
Part Number: TLC6C5716-Q1 Hi,
We are using TLC6C5716-Q1 16 channel-LED Driver.
While trying to drive the any o/p channel we are getting ERROR Pin-20 signal (Active Low).
Below are the steps which we are following in firmware
1) LED_ERR_MASK is SET to Zero…
Part Number: TLC6C5716-Q1 Hello, Team,
We have question about grayscale configuration. We would like to dimming with 200Hz,
Our understanding is that in order to do so, we need to input GCLK and set the ON pulse of PWM using resister.
When using 200Hz…