Part Number: TLE2426 Hi, I see obsolescence of all p/n's TLE2426, specifically TLE2426CD.
But regarding the final DATE for Last buy I found 2 PCN with different date in my opinion
PDN Number: 20230907000.3 PDN Date: September 07,2023
reports only…
Part Number: TLE2426 I see that Mouser has not tagged TLE2426QDRG4Q1 as 'end of life', unlike the other variants. Will the TLE2426QDRG4Q1 also be soon tagged 'End of Life'?
Will there be no SOIC-8 variants of TLE2426 available in the near…
Part Number: TLE2426 Hey team,
I got a customer inquiry regarding the TLE2426 that's going EOL for a suitable replacement. I'll copy the email below.
"It appears the TLE2426 family is going EOL as stated on PDN 20230907001.3. HME engineering…
Part Number: TLE2426
[Case:657239]Technical Data Inquiry for our customer.
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance.
Please confirm if this part TLE2426IDRG4 is Obsolete.
Part Number: TLE2426 HI all,
I'm trying to realize a simple 2 x audio splitter using TLE2426 IC to have a dual power supply froma a single one.
Am I on the right way?
Thank all for support,
Leonard
Part Number: TLE2426 Hello,
Our customer try to substitute of TLE2426 by TLE2426-Q1 as expecting upper compatibility.
When we compared specification of Output voltage regulation at -10mA sourcing condition TLE2426-Q1 is -0.102mV and Non-Q1 has -45uV,…
Part Number: TLE2426 The SPICE model for TLE2426 doesn't work with floating circuit simulations, see below. V+ should be 5V, and V- should be -5V. There should be NO CURRENT in the output of the '2426.
I compared this with an equivalent circuit…
Part Number: TLE2426 Other Parts Discussed in Thread: OPA1637 Hello I am Jung
I am using TLE2426 for DAC to supply 8pcs of OPA1637 for VOCM.(Mid bias)
I found a problem which is the output of TLE2426 is only 0.7V.(I expected 2.5V because input voltage…
Part Number: TLE2426 I would like to see a basic circuit diagram which incorporates proper use of a TLE2426 to bias the non-inverting input of an opamp to half the V+ power supply voltage
Part Number: TLE2426 Dear Texas Instruments
I purchased TLE2426CLPR via Digikey.
I thought that TLE2426CLPR is TO-92 (straight lead (leg)),
but I got formed lead type instead of straight lead type.
If I'd like to get straight type, what part number should…