Part Number: TLK10034 The data sheet did not provide power design information. Is there a app note, design guide or reference design you could send me with recommendations?
Is a separate regulator needed for the analog core?
Would a single supply with…
Part Number: TLK10034 Hello,
My customer is asking if there are register settings that can be read that provide the RX adaptive equalization settings being applied to the device. I see that bits 11:8 in register 0x0008 correspond with LS Serdes Equalization…
Part Number: TLK10034 Other Parts Discussed in Thread: MSP430F5529 Hi
I am trying to use USB-2MDIO GUI to talk to TLK10034. The LaunchPad I use is MSP430F5529.
I connect external 1.8V to the MSP430F5529.
When I try to read or write through GUI, it always…
Part Number: USB-2-MDIO Other Parts Discussed in Thread: TLK10034 , MSP430F5529 Hello,
My customer is looking to use the USB-2-MDIO GUI and MSP430F5529 LaunchPad to communicate with TLK10034. They're able to read registers from the TLK10034, however, they…
Hi Rodrigo,
I have checked the potential issue. For MDIO, I use an opain-drain level shifter (LSF0102DCU) (The TLK10034 having a MDIO bus referenced to 1.8V, the ethernet switches bus referenced to 3.3V).On the TLK10034 side I have pull-ups of 2kOhm on…
Part Number: TLK10034 Other Parts Discussed in Thread: TLK10232 Hello,
I am using the TLK eval board.
There is 4 10G channel available with my board (Lane A, B, C and D).
My objective is to use 10GBaseKR, with autoneg and training.
When i loopback lane…
Part Number: TLK10034 For a poor PCB layout we're unfortunately stuck with, we've found that lowering the VDDA voltage below its 1.0V +/-5% spec gives us reliably good performance, so far over temperature as well. VDDT, DVDD & VDDD are still at…
Part Number: TLK10034 Hi,
We are looking for a Quad Port XAUI to 10GBASE-R/XFI converter device for below application,
Processor/MAC with XAUI interface <---> TLK10034 with XAUI interface at host side & 10G-BASE-R at line side <---> Mult-rate…
Part Number: TLK10034 Are there any common 10G performance issues root caused to part handling? We continue to see high variance in packet errors CCA to CCA.
Part Number: TLK10034
I have a PCB design where 4 - TLK10034 's are implemented. This effectively produces 16 channels on my PCB. The LS side of the device uses the XAUI interface. The HS side feeds a 10G optical transceiver. For 14 out of the 16 channels…