Part Number: TLV1117 Dear Sir/Madam,
We are using TLV1117CDCYR, adjustable LDO regulator, in our project. When the load to output of this LDO regulator is removed, the OUTPUT pin is 1.31V greater than ADJUST pin. But when there is load current 15mA…
Part Number: TLV1117TLV1117IDRJR in the datasheet you give a thermal resistor from chip to ambiente for 38K/W. With this number a abient temperature I get a max Power of 2,8W. When I try to calculate with the calculation tool from TI I need a spread…
Part Number: TLV1117-33 Dear Linear Regulators team
I want to have LDO(Input: 12V, Output: 3.3V@100mA ) + LIN Transceiver Function.
However, I can't search web site.
Do you have LDO with LIN Transceiver Function of TI item?
Thanks
Best…
Other Parts Discussed in Thread: TLV1117 Dear Sir
May I know TLV1117 could replace G1117 directly or I need to change the input can output cap as well??
Due to we have some of project use Vin=12V in old project ,so we want to use TLV1117 instead…
Part Number: TLV1117 Hi team,
Could you please provide the thermal model of TLV117? One of my customers need it the do thermal simulation in Flotherm.
Thanks.
Best regards,
Dongbao
Other Parts Discussed in Thread: TLV1117 I want to know about TLV1117.
Can I use ceramic capacitor when I choose output capacitor of TLV1117.
Best regards,
Part Number: TIDA-00951 Hi!
We have developed the PCB and while testing we encountered the following error in the board :
The IC U12 - TLV1117-33IDRJR should give 3.3V output from input of 5V. But it doesnt seem to give the expected output. When we…