Part Number: TLV1701-Q1 Other Parts Discussed in Thread: TLV1701 , TLV1821 Hello team,
My customer is reviewing the worst case calculate of TLV1701, please help review the questions as below.
1. How to understand the direction of input bias current? Can…
Part Number: TLV1701-Q1 Other Parts Discussed in Thread: TLV1811-Q1 , TLV1805-Q1
We have designed the non-inverting comparator using TLV1701QDBVRQ1 part. Our circuit need to give +/- 12V PWM output based on the input. We are seeing the slew rate issue…
Part Number: TLV1701-Q1 hi team,
Could you help work out a suitable solution to fit in below application?
Input signal: 10Hz PWM, voltage range from 0V to 18.5V
Output signal: logic low when VIL:0~2 V, logic high= VLH:4.2-18.5V
Regards,
Dongbao
Part Number: TLV1701-Q1 Hello team,
What the package difference between SC70 and SOT-23? Do you have any doc to compare these 2 packaged to see the advantages and disadvantages?
Thank you,
Lanxi
Part Number: TLV1701 Other Parts Discussed in Thread: TINA-TI May I know what is the max current in pin5 and pin4?
We would like to know how much will TLV1701AIDRLT can consume from +PW_VCC3V3_LDO?
Part Number: TLV1701 Hi Experts,
Seeking your assistance on this query:
The part number in question is TLV170x - 2.2V to 36V microPower Comparator. We're supplying the chip with 24V, using the comparator as an overvoltage sensor (Estop circuit). The…
Part Number: TLV1701 Other Parts Discussed in Thread: LM139 My customer sees issues with the TLV1701 Pspice model when running it on his licensed Cadence Pspice platform (not Pspice for TI). The model does not converge or seems to just hangs for many…
Part Number: TLV1701-Q1 I have a question regarding the TLV1701QDBVRQ1 absolute max signal input levels.
The datasheet specifies that the maximum signal input voltage is (Vs+) + 0.5, and the maximum input current is ±10mA.
Note 2 also states that…