Part Number: TLV1702 Good afternoon,
We have order the TLV1702 at Digi-Key and wating for more than a year for this component.
Is it possible to get a real delivery time?
Kind regards,
Frans
Part Number: TLV1702 Hello,
We received PCN 20220512000.1 which brought up some questions, in particular about P/N TLV1702AIDGKR.
Can you please confirm if part TLV1702AIDGKR currently has NiPdAu or NiPdAuAg terminal finish? Which ( NiPdAu or NiPdAuAg ) has…
Part Number: TLV1702 Other Parts Discussed in Thread: LM2903B , LM2903 , LM393 , LM393B , Hi TI,
I am using TLV1702AIDGK in my design. The design is intended for current and voltage measurement. And I use this chip for over voltage/over current protection…
Part Number: TLV1702 Other Parts Discussed in Thread: LM393 , LMC6772 , LM339
I have a resistor meter with LCD display and ICL7106 AD.
The ICL7106 is quite low resolution 3.5 digits.
I need more from 0.0 ohm to 1999 ohms.
I have made a external range switch…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1701 Hi team,
My customer requires spice model for TLV1702-Q1.
Can we propose Pspice model of TLV1701 instead?
Best regards,
Part Number: TLV1702
hi Sir/Miss,
I am performing electrical analysis on a circuitry using this comparator TLV1702AQDGKRQ1 but could not find the Input Offset Current across -40C to 125C.
May I know what would be the recommended max Input Offset Current…
Only the LM2903 and LM2903-N match these requirements.
As bipolar devices, the LM2903(-N) consume about 0.8 mA (total for both comparators). If you want to use a power-saving CMOS device like the TLV1822 or TLV1702, you need to use an SMD-to-DIP adapter…
Part Number: TLV1702 Other Parts Discussed in Thread: , TLV7022 We are using samples TLV1702-Q1 for our design with 5V supply and pull up resistor of 1k ohm.
Of the dual comparators, one is working fine but the second gives a high output of around 2-2…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV7022 , TLV7012 Hi Team,
We are looking in for AC over current sensing application of a 3 phase motor inverter.
Current transducer output is from 0.5V to 4.5V.
Over current threshold limit: 1V…